Announcements

Learn how to optimise USB-C for your designs at 18 May's USB-C PD Webinar.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

OlEr_1999891
Level 5
Level 5
50 replies posted 25 replies posted 25 sign-ins

Hi!

We are looking (again) at developing a DisplayPort 1.2 Input + USB 3.0 Input to USB-C (DFP) adapter. The CCG3 Host reference design is more or less the design we are looking at, but we had one key question:

If we want to allow Pin Assignment D (2 lanes DP and 2 lanes USB 3), will that work when a upstream laptop is connected via legacy DisplayPort 1.2 cable? Will that laptop get information via AUX that it should provide only 2 lanes DP? Since the laptop will not be part of the PD signalling regarding C or D pin assignment. 

What we "fear" is that the laptop will always default to 4 lanes DP on the DP output and not be informed about the need to only deliver 2 lane DP on lane 0 and 1. 

Since Cypress host reference design has a DP 1.2 input and it apperently works when connecting a laptop via a DP cable to it, maybe it is not a problem?

Cheers

Olof

3 Replies
ShifangZ_26
Moderator
Moderator
Moderator
10 likes given 250 sign-ins 1000 replies posted

Hi Olof,

If this product is going to integrate into Notebook/Laptop board directly, there is no problem. Since CCGx could have communication with EC to get more details information about the DP source selection.

Typically, The source side will offer more pin assignments options and select the best one as per attached device. If you are a dongle only, and you specified to 2 lane DP and USB3.0, the UFP_D may not support it. This will be a compliance issue. 

Actually, CCG3 C to DP cable is bi-direction solution already, it is cover your case. Am I correct?

 

Best Regards,

Lisa

0 Likes
OlEr_1999891
Level 5
Level 5
50 replies posted 25 replies posted 25 sign-ins

Hi Lisa!

It is ok that the dongle support both C and D assignments so ensure compliance. Our worry is that the laptop with the DP source will not be informed correctly that is should serve 2 or 4 lanes DP since CCGx in this case will not be able to communicate with the laptops EC/GPU. 

CCG3 C to DP doesn't support USB 3 right? And our adapter needs a Type-C receptacle, not a plug so we need to mux for that reason as well.

The question is if the laptop (DP Source) via the AUX lane via the DP cable will get the correct information to serve 2 or 4 lanes.

Cheers

Olof

0 Likes
ShifangZ_26
Moderator
Moderator
Moderator
10 likes given 250 sign-ins 1000 replies posted

Hi Olof,

It is difficult to get the correct information to identify attached DP sink is 2 lane or 4 lane via AUX channel.

 

Best Regards,

Lisa

0 Likes