- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi!
When I copy and compile the standard CYPD3125-40LQXI_notebook.cydsn project from the 3.4 Host SDK both backup_fw and main fw compiles without problem. However, when I change to CYPD3123 (via Device Selector) and change the bootloader to "CYPD3123-40LQXI_usb_boot_3_0_2_900_0_0_0_cu.hex", I get:
ERROR: cannot open linker script file .\cm0g_1.ld: No such file or directory
collect2.exe: error: ld returned 1 exit status
The command 'arm-none-eabi-gcc.exe' failed with exit code '1'.
when building the project. Tried without success:
- Renaming cm0gcc.ld to cm0g_1.ld, but there was no cm0gcc_2.ld in the project folder
- Copy cm0g_1.ld / cm0g_2.ld from the backup_fw projet
Do I need a new USB bootloader file for the 3.4 SDK? Or does the linker-files need to change to fit in the USB booatloader?
Cheers
Olof
Solved! Go to Solution.
- Labels:
-
USB EZ-PD Type-C
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Olof,
1. You shall update the usb boot in Application FW2 only same as Host SDK and make sure back up project have been complied successful.
2.. If you are using MDK complier with host SDK3.4, your question is correct, the CYPD3123 usb boot need a new .elf and .hex file for usb boot.
Best Regards,
Lisa
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Olof,
1. You shall update the usb boot in Application FW2 only same as Host SDK and make sure back up project have been complied successful.
2.. If you are using MDK complier with host SDK3.4, your question is correct, the CYPD3123 usb boot need a new .elf and .hex file for usb boot.
Best Regards,
Lisa
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Lisa!
Thanks for the answer. Where do we find the usb bootloader binaries for 3.4?
Cheers
Olof
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Olof,
Currently, there is not release candidate of usb bootloader binaries for 3.4. Recommend you use I2C bootloader and enable billboard for dock design.
Best Regards,
Lisa
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Ok. We use CYPD3123 in our devices, not in the dock. That is why we need USB Bootloader. Ok, we stick with the older EZ-PD SDK. Pls consider releasing a 3.4 binary of the USB Bootloader.
Cheers
Olof
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Olof,
Sure. We will consider releasing a 3.4 binary of the USB Bootloader. Thank you very much for your feedback.
Best Regards,
Lisa