- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello community,
I'm using CCG3PA for my product development.It can act as only PD/QC Sink.
So to verify Qc 2.0 Sink Functionality I'm using miniprog and Bridge control utility to initiate commands over I2C and perform required actions.
I want to apply Pull-up or Pull-down on Dp/Dm lines as per QC2.0 protocol, so I've added below function in pdss_mx_hal.c and calling whenever required, also I will be calling bc_init(0); and chgb_enable(0); explicitly before starting QC2.0 functionality :
ccg_status_t grl_chgb_apply_sink_term(uint8_t cport, grl_chgb_snk_term_t charger_term)
{
PPDSS_REGS_T pd = gl_pdss[cport];
switch(charger_term)
{
case PULL_UP_DP://0
pd->bch_det_0_ctrl[cport] |= PDSS_BCH_DET_0_CTRL_RDP_PU_EN;
break;
case PULL_UP_DM://1
pd->bch_det_0_ctrl[cport] |= PDSS_BCH_DET_0_CTRL_RDM_PU_EN;
break;
case PULL_DOWN_DP://2
PDSS->bch_det_0_ctrl[cport] |= PDSS_BCH_DET_0_CTRL_VDP_SRC_EN;
break;
case PULL_DOWN_DM://3
pd->bch_det_0_ctrl[cport] |= PDSS_BCH_DET_0_CTRL_VDM_SRC_EN;
break;
case REMOVE_TERMS://4
chgb_remove_term(cport);
break;
case VBUS_5V://5
/* 0.6 on D+, D- HiZ */
PDSS->bch_det_0_ctrl[cport] |= PDSS_BCH_DET_0_CTRL_VDP_SRC_EN;
/ * Remove other terms */
PDSS->bch_det_0_ctrl[cport] &= ~ (PDSS_BCH_DET_0_CTRL_RDP_PU_EN |
PDSS_BCH_DET_0_CTRL_RDM_PU_EN |
PDSS_BCH_DET_0_CTRL_VDM_SRC_EN |
PDSS_BCH_DET_0_CTRL_IDM_SNK_EN);
break;
}
return CCG_STAT_SUCCESS;
}
So I will be initiating commands over I2C from bridge control utility with
Case A: Power being 3.3v in utility,
Case B: Power being 5v in utility.
In case A with input power supply to ccg3pa IC being 3v3 when I apply Pull-up on Dp/Dm line I'm seeing only ~2.75v (in multi-meter)on Dp0(TP9)/Dm0(TP12) physical available pins on DVK because of which Connected QC2.0 provider is unable to change its voltages from one range to other range, which is unexpected.
In case B with input power being 5v, I'm seeing around ~4.4v on Dp0(Tp9)/Dm0(Tp12) lines because of which DUT is changing its Vbus voltage from one range to other range which is expected.
Problem statement:
-->Provider is not changing its Vbus voltage from one range to the other range as the Dp/Dm voltage ranges are out of the tolerance value of Dp/Dm line validation range by a Provider DUT to change its Vbus voltage.
Q1: Is this sequence expected as per CCG3PA design ?
Q2: If expected, Do we Anyway to make this work at 3.3v input.
Thanks and regards,
Pranay.
Solved! Go to Solution.
- Labels:
-
USB EZ-PD Type-C
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Pranay!
This should not be the case. When you apply termination it should be pulled up to appropriate voltage without any drop.
Can you try disabling all other terminations using ccg_status_t chgb_remove_term(uint8_t cport) before applying the termination required and check if the behavior changes?
Pranava