Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB EZ-PD™ Type-C Forum Discussions

PaRi_1293246
Level 3
50 sign-ins 10 questions asked 25 sign-ins
Level 3

Hello,

I have installed Keil MDK v5.26 in order to get the ARMCC compiler.  When I built the 'CYPD3125-40LQXI_notebook' project,  that is the project for the CCG3 evaluation kit, I get an error related to cyelftool.exe that cannot be located.

Here is the message:

C:\IIM\Echo700\USB Type-C Controller\Firmware\Revision G0\CYPD3125-40LQXI_01-Test\CYPD3125-40LQXI_notebook\CYPD3125-40LQXI_notebook.cydsn>cyelftool.exe -M CortexM0\ARM_MDK_Generic\Debug\CYPD3125-40LQXI_notebook.elf backup_fw.cydsn\CortexM0\ARM_MDK_Generic\Debug\backup_fw_1.elf CortexM0\ARM_MDK_Generic\Debug\CYPD3125-40LQXI_notebook.hex --flash_row_size 128 --flash_size 131072 --flash_array_size 131072
'cyelftool.exe' is not recognized as an internal or external command,
operable program or batch file.
"Post-Build Script failed: could not locate cyelftool.exe"
The command '.\post_build.bat' failed with exit code '9009'.

How can I repair that error?

Thank you

Best Regards,

Patrice

0 Likes
1 Solution
Wang_Fred
Moderator
Moderator 25 replies posted 10 solutions authored 50 sign-ins
Moderator

Hello  Patrice,

Is the 'CYPD3125-40LQXI_notebook' project is from EZ-PD CCGx Host SDK v3.4?

If yes, please refer to the content of pag#20 (item#8) in CCGx_Host_SDK_UserGuide to eliminate this compile error. 

This doc existing under directory(by default) - C:\Program Files (x86)\Cypress\EZ-PD CCGx Host SDK\CCGx\Documentation

Thanks,

Fred

View solution in original post

0 Likes
1 Reply
Wang_Fred
Moderator
Moderator 25 replies posted 10 solutions authored 50 sign-ins
Moderator

Hello  Patrice,

Is the 'CYPD3125-40LQXI_notebook' project is from EZ-PD CCGx Host SDK v3.4?

If yes, please refer to the content of pag#20 (item#8) in CCGx_Host_SDK_UserGuide to eliminate this compile error. 

This doc existing under directory(by default) - C:\Program Files (x86)\Cypress\EZ-PD CCGx Host SDK\CCGx\Documentation

Thanks,

Fred

0 Likes