- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi am looking for any example in Power SDK or Host SDK of implemnet I2C SCB block as I2C slave usage byte level APIs
all examples which i found or community support refer me to is master
could you please refere me to slave i2c scb block in usage byte level APIs it will help me reduce size of my application
Solved! Go to Solution.
- Tags:
- cypd3175

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi,
Currently, we dont have such an example and to access the data as I2C slave byte by byte, you will have to implement a custom ISR that would detect the bus events properly and do a read from FIFO or write to FIFO based on bus direction. You could refer to the I2C_INT.c file and implementation in the I2C interrupt for the SCB under Generated Source for reference.
Best Regards,
Sananya

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi,
Please refer to the HPI_IF component in the CYPD3125-40LQXI_notebook project in the Host SDK for I2C slave SCB component. The SCB APIs are not directly used in the project so you could refer to the code example https://www.cypress.com/documentation/code-examples/ce224599-psoc-4-i2c-slave-serial-communication-b... to check the APIs that can be used with the same I2C slave SCB component.
Best Regards,
Sananya

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi ,
i dont want tu use HAL of I2C Slave SCB block sach as I2CS_I2CSlaveClearReadBuf i want use like this alnog with timer this example below is master i didnt succses find like this as slave could you provide example ?
uint32_t i;
uint8_t status = false;
i2c_state = CyEnterCriticalSection();
/* Clear the timeout flag and start a timer. */
mux_xfer_timeout = false;
timer_start (0, MUX_I2C_TIMER, MUX_I2C_TIMER_PERIOD, mux_xfer_timer_cb);
/* If the bus is free, generate a Start condition. */
if ((I2CM_I2C_STATUS_REG & I2CM_I2C_STATUS_BUS_BUSY) == 0)
{
/* Assume operation passed for now. */
status = true;
/* TX and RX FIFO have to be EMPTY. */
I2CM_TX_FIFO_WR_REG = (uint32_t)(addr << 1); /* Put address in TX FIFO. */
I2CM_ClearMasterInterruptSource (I2CM_INTR_MASTER_ALL);
I2CM_I2C_MASTER_GENERATE_START;
/* Wait for an ACK from the MUX. */
while (!I2CM_CHECK_INTR_MASTER(I2CM_INTR_MASTER_I2C_BUS_ERROR |
I2CM_INTR_MASTER_I2C_ACK |
I2CM_INTR_MASTER_I2C_NACK |
I2CM_INTR_MASTER_I2C_ARB_LOST) &&
(!mux_xfer_timeout));
/* Transfer the remaining data out to the MUX. */
for (i = 0; ((!mux_xfer_timeout) && (i < count)); i++)
{
/* Clear ACK interrupt from earlier. */
I2CM_CLEAR_INTR_MASTER (I2CM_INTR_MASTER_I2C_ACK);
I2CM_TX_FIFO_WR_REG = buffer;
while (!I2CM_CHECK_INTR_MASTER(I2CM_INTR_MASTER_I2C_BUS_ERROR|
I2CM_INTR_MASTER_I2C_ACK |
I2CM_INTR_MASTER_I2C_NACK |
I2CM_INTR_MASTER_I2C_ARB_LOST) &&
(!mux_xfer_timeout));
}
}
/* Send a STOP to the slave. */
I2CM_I2C_MASTER_GENERATE_STOP;
while (!I2CM_CHECK_INTR_MASTER(I2CM_INTR_MASTER_I2C_STOP |
I2CM_INTR_MASTER_I2C_ARB_LOST |
I2CM_INTR_MASTER_I2C_BUS_ERROR) &&
(!mux_xfer_timeout));
/* Check the results of the address phase. */
if (I2CM_CHECK_INTR_MASTER (I2CM_INTR_MASTER_I2C_NACK |
I2CM_INTR_MASTER_I2C_ARB_LOST |
I2CM_INTR_MASTER_I2C_BUS_ERROR) ||
(mux_xfer_timeout))
{
/* Transaction failed. Reset the SCB block and return error. */
I2CM_CTRL_REG &= ((uint32) ~I2CM_CTRL_ENABLED);
I2CM_CTRL_REG |= ((uint32) I2CM_CTRL_ENABLED);
status = false;
}
timer_stop (0, MUX_I2C_TIMER);
CyExitCriticalSection(i2c_state);
return (status);

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
i want reduce-i2c-scb-block-usage- to byte-level

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi,
Currently, we dont have such an example and to access the data as I2C slave byte by byte, you will have to implement a custom ISR that would detect the bus events properly and do a read from FIFO or write to FIFO based on bus direction. You could refer to the I2C_INT.c file and implementation in the I2C interrupt for the SCB under Generated Source for reference.
Best Regards,
Sananya