- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
How ist it possible to read the logic level on the configuration channel pins CC1 and CC2 of the CCG3 PSoC in PSoC Creator?
In the Pins view it looks like the pins CC1 and CC2 can't be configured like other GPIOs:
I am using the CYPD3125 in a one chip solution, where I need to control a USB C MUX dependant on the USB C connector rotation. As this is my first project with USB and PSoC, I don't have any previous knowledge in this area.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi ,
If you are going to use I2C controlled MUX, the CYPD3125 example code file datamux_ctrl.c is the source file containing the data MUX (PS8740) control functions for the CCG firmware application. You could refer it directly.
Of course, if you just want to know how to get the CC1 is used as CC or CC2 is used as CC, below function can be used.
/**
* @brief Get the CC polarity of the Type-C connection.
* @param port Port index.
* @return Returns 0 if CC1 is used, and 1 if CC2 is used.
*/
uint8_t dpm_get_polarity(uint8_t port);
Best Regards,
Lisa