Failed to Build CCG3x Example with ARM-CC in PSoC Creator 4.5

Announcements

Live Webinar: USB-C adoption. Simple & Cost-efficient solutions | April 18th @9am or 5pm CEST. Register now !

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
txcao
Level 3
Level 3
10 replies posted 50 sign-ins First solution authored

- Example code: Any example code for CYPD3120 or CYPD3123

- PSoC version: 4.4 or 4.5

- PSoC IDE setting
+ If using default ARM toolchain: ARM GCC 5.4-2016-q2

-> Error: Build error:

Build error: passing argument 1 of 'memset' discards 'volatile' qualifier from pointer target type [-Werror=discarded-array-qualifiers]

+ If using MDK533

-> Error: 

 

 

cannot open source input file "stack_params.h": No such file or directory
  #include <stack_params.h>

 

 

 We got error messages even we use default GCC or MDK. Could you help to solve the problem?

0 Likes
1 Solution
ShifangZ_26
Moderator
Moderator
Moderator
10 likes given 250 sign-ins 1000 replies posted

Hello ,

CCGx example code of CYPD3120/3123 from CCGx SDK 3.0.2 is based on ARM GCC 4.9-2015-q1-update complier Toolchain. Please feel free to download PSoC Creator 3.3 based on this project and re-build firmware project directly without MDK Toolchains manually configure. 

 

ShifangZ_26_0-1678678570449.png

Best Regards,

Lisa

View solution in original post

0 Likes
1 Reply
ShifangZ_26
Moderator
Moderator
Moderator
10 likes given 250 sign-ins 1000 replies posted

Hello ,

CCGx example code of CYPD3120/3123 from CCGx SDK 3.0.2 is based on ARM GCC 4.9-2015-q1-update complier Toolchain. Please feel free to download PSoC Creator 3.3 based on this project and re-build firmware project directly without MDK Toolchains manually configure. 

 

ShifangZ_26_0-1678678570449.png

Best Regards,

Lisa

0 Likes