- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
We have implemented on our new ultrasound scanner an USB C port based on the CYPD3125-40LQXI controller. We are running the firmware that come from the EZ-PD CCGx Host SDK CYPD3125-40LQXI-notebook project. We have one Source PDO (5V/1500mA) and two Sink PDO (5V/900mA and 15V/3000mA).
When we connect an USB C power adapter to our ultrasound scanner the USB C controller request the 15V and turn on the consumer path. It's working has expected.
When we add an USB C hub with power delivery between the USB C power adapter and our ultrasound scanner the output of the power adapter stay at 5 volts and the USB C controller doesn't turn on the consumer path. The two USB C hub that we have tried (one 60W and one 100W) behave the same way.
Is the firmware from the EZ-PD CCGx Host SDK CYPD3125-40LQXI-notebook project compatible with the used of an USB C hub with power delivery? Do I need the modify the default configuration?
Thank you
Best Regards,
Patrice
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Practice,
May I know which kind of USB C hub you used? Is there a power input port from external power adapter and a power output port (to e.g. your scanner)?
BTW, is it possible to capture the cc log between the scanner and USB C hub as well as the cc log between power adapter and USB C hub?
Thanks,
Fred
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Fred,
The two USB C hub that I have tried have a power input port from the USB C power adapter and a power output that is the USB C port that I connect to our system. I have successfully tested both of them to charge my cellular phone.
I have ordered a CY4500 EZ-PD Protocol Analyser to capture the traffic on the two CC bus. I will get back to you as soon I receive it.
Best Regards,
Patrice