- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi, I would like to confirm if every cypress PD Device CYPD6227-96BZXI programmed with basic firmware when the part is shipped out from cypress factory. What are the basic functions of this firmware?
https://www.cypress.com/part/cypd6227-96bzxi
-Kiran
Solved! Go to Solution.
- Labels:
-
USB EZ-PD Type-C
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
The default factory firmware and bootloader for CCG6 chips are as below,
CCG6 | ||
Part Number | Default Application Firmware | Bootloader |
CYPD6127-48LQXI | Notebooks | I2C Bootloader |
CYPD6128-48LQXI | I2C Bootloader | |
CYPD6227-96BZXI | I2C Bootloader | |
CYPD6228-96BZXI | I2C Bootloader |
This default firmware would be preprogrammed before shipping.
CCG6DF 96-BGA Dual Port Thunderbolt Notebook Application: The CCG6DF device communicates with the embedded controller (EC), which manages the Battery Charger Controller (BCC) to control the charging and discharging of the internal battery. It also updates the Thunderbolt Controller via I2C to route the High Speed signals coming from the Type-C port to the USB host (during normal mode) or the Graphics processor unit (during Display port Alternate mode) or the Thunderbolt Host (during Thunderbolt Alternate mode) based on the alternate mode negotiation. The CCG6DF device controls the transfer of USB 2.0 DP and DM lines from the top and bottom of the Type-C receptacle to the DP and DM lines of the USB Host controller. CCG6DF offers VBUS Short protection on SBU and CC lines. The CCG6DF device has integrated VCONN FETs for applications that need to provide power for accessories and cables using the VCONN pin of the Type-C receptacle. The 5-mohm resistor between the 5-V supply and the integrated provider FETs is used for overcurrent detection on the VBUS.
For more details please refer the CCG6DF datasheet.
Regards,
Abhilash P