Compile error with Creator 4.1

Announcements

Live Webinar: USB-C adoption. Simple & Cost-efficient solutions | April 18th @9am or 5pm CEST. Register now !

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hello,

I tried to compile SDK sample code of CYPD3125-40LQXI_notebook with Creator 4.1.

CCGx FW UserGuide described, "This version of the SDK requires PSoC Creator 3.3 DP1 (build 9674) or higher".

At first, I update all of the components used in the project to latest version.

Next, I set up the option for ARM MDK Generic.

Finally, build it.

Also, I could build the project with Creator 3.3.

Creator shows many errors below. So please let me know how I can resolve them.

1) Build error: error: lto-wrapper failed

2) Build error: The command 'arm-none-eabi-gcc.exe' failed with exit code '1'.

3) The instance 'HPI_IF', of component SCB_P4_v3_10, contains an error. Unable to locate and customize component 'SCB_P4_v3_10' used in schematic

4) The instance 'MUX_CTRL', of component SCB_P4_v3_10, contains an error. Unable to locate and customize component 'SCB_P4_v3_10' used in schematic

5) The fitter aborted due to errors, please address all errors and rebuild.

Best regards,

0 Likes
1 Solution
ShifangZ_26
Moderator
Moderator
Moderator
10 likes given 250 sign-ins 1000 replies posted

Hi Takeshi,

You are correct that the SDK3.0.2 has to be used with Creator 3.3 DP1. There will not compiling error will be pop-up.  This error show up for Build error: error: lto-wrapper failed is because the gcc compiler is changed from 3.3 to 4.1, and CCGx 3.0.2 is released before Creator 4.1. I am checking if there is anyway to link the compiler of Creator 3.3 DP1 to Creator 4.1 to help out this issue.

For other errors, you could update all of components to latest one will fix it.

Best Regards,

Lisa

View solution in original post

0 Likes
4 Replies