- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi
I can't update any firmware on the CYPD3175 chip because of this error:
When connecting CY4532 kit to program the CYPD chip and go through "Tools --> Firmware update" and select the "CYPD3175-24LQXQ_pa_direct_fb\CYPD3175-24LQXQ_pa_direct_fb_3_5_0_2649_0_0_0_pa.cyacd" file the upload gets to 99% and then I get this error message:
PD contract established.
Restarting the target device
Re-negotiating PD contract after switching target reset
PD contract established.
Device is in boot mode: Starting FLASH update operation
Programming data from file: C:\Program Files (x86)\Cypress\EZ-PD CCGx Power SDK\CCGx\Firmware\binaries\CYPD3175-24LQXQ_pa_direct_fb\CYPD3175-24LQXQ_pa_direct_fb_3_5_0_2649_0_0_0_pa.cyacd
Firmware/Configuration write to flash completed
Firmware image (FW:1) is valid
Restarting the target device
Re-negotiating PD contract after switching target reset
Error: PD contract not established after RESET
Error: Flash update procedure failed
Error: DLL call returned error while flashing
I'm using Power Boar as a programmer:
Any suggestion how to solve it?
It will be e great help.
Thank you
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Please refer to the thread programming CCG3PA from CY4532 EVK.
From the error message it can be seen that on the 8th line it says "Firmware/Configuration write to flash completed " .
This error message comes up because the new firmware which was written to flash is unable to start since the jumper settings have not yet been changed to support the new firmware.
Hence the error message displayed on the dialog box “Firmware/Configuration upgrade not completed. Refer to the message window for details” seen in the EZ-PD Configuration Utility GUI can be ignored. You can change the jumper settings according to the new firmware and everything works fine.
Please change the jumper settings according to your new firmware and cross check if the firmware is updated using "firmware read" option available in the EZ-PD Configuration utility,
For more details please refer the EZ-PD CCG3PA EVK guide .
Please revert back if you are unable to read the firmware.
Regards
Abhilash P