Can cypd3135 bootloader code be used on cypd3125?

Announcements

Live Webinar: USB-C adoption. Simple & Cost-efficient solutions | April 18th @9am or 5pm CEST. Register now !

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
GrCa_1363456
Level 6
Level 6
50 likes received Beta tester First comment on KBA

I purchased CYPD3125 parts but now want to use CC bootloader instead of i2C.

CYPD3125 comes with i2C bootloader pre-installed.

CYPD3135 comes with cc bootloader pre-installed.

The compiled hex and elf files for CYPD3135 are available by downloading the example for CYPD3135 in PSoC Creator.

Will the compiled CYPD3135 code work in a CYPD3125?

If not should I start with CC boot code from CYPD2134, a CCG2 part that comes with cc bootloader source and complied code, then re-compile it for the CYPD3125?

0 Likes
1 Solution
ShifangZ_26
Moderator
Moderator
Moderator
10 likes given 250 sign-ins 1000 replies posted

Hi

The cc bootloader project along with CYPD3135 could change Device part number from CYPD3135 to CYPD3125. After re-build it, you could get a cc bootloader hex and elf suit for CYPD3125.

If you use the CYPD3135 hex and elf file directly, the bootloadable will not able to work with silicon mismatch error.

The CCG2 device flash size is difference with CCG3 device. Please kindly notice that.

Best Regards,

Lisa

View solution in original post

0 Likes
1 Reply
ShifangZ_26
Moderator
Moderator
Moderator
10 likes given 250 sign-ins 1000 replies posted

Hi

The cc bootloader project along with CYPD3135 could change Device part number from CYPD3135 to CYPD3125. After re-build it, you could get a cc bootloader hex and elf suit for CYPD3125.

If you use the CYPD3135 hex and elf file directly, the bootloadable will not able to work with silicon mismatch error.

The CCG2 device flash size is difference with CCG3 device. Please kindly notice that.

Best Regards,

Lisa

0 Likes