- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
I am working with a CYPD6125 and am trying to use the SBU1 and SBU2 pins as a side band communications channel between two devices. I see a few mentions in the CYPD6125 TRM that the chip contains an SBU mux that can be set so that the AUX_P and AUX_N pins are connected to the SBU pins. However, I have not been able to find any support or examples showing how to configure that mux.
What functions or registers should I be using to set the SBU pins to be driven by the AUX pins, and is there a document or sample project that details how to use them?
Solved! Go to Solution.
- Labels:
-
USB EZ-PD Type-C

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi,
As you have pointed out, mux_ctrl_set_cfg() is in turn called by set_mux() function. This set_mux() function is used to configure the mux at multiple places.
You can disable mux control by changing the MUX_TYPE macro present in solution.h to value other than DP_MUX. This will disable the control of this message through all parts of code.
>> For port value, you can use this macro - TYPEC_PORT_0_IDX
If so, where should this invocation take place? Should I be manually adding it to the initialization section of my main.c?
>> Yes
Pranava

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi,
I believe you are using CYPD6125-40LQXI_notebook project from CCGx Host SDK.
You can refer to mux_ctrl_init() and mux_ctrl_set_cfg() functions present in solution.c file. By default, all necessary MUX switching is taken care by the SDK code. May I know why you would want to use this MUX manually?
Pranava
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
> May I know why you would want to use this MUX manually?
I don't plan to use this connection for DisplayPort or Thunderbolt, so I intend to use the SBU pin as a GPIO for sideband communication to a microcontroller connected to AUX_N of my downstream CCG6.
I have two devices, each of which has a CCG6 on board. My goal is for my upstream device to set the AUX_N/P of the upstream CCG6 high when it needs to the downstream device to enter a special operation mode, which will then cause the downstream CCG6's AUX_N/P pin to go high. My downstream MCU will see the AUX_N/P pin go high, and enter its special operation mode.
> You can refer to mux_ctrl_init() and mux_ctrl_set_cfg() functions present in solution.c file.
Thank you for pointing me in the right location for this function. The documentation seems rather lacking for the mux_ctrl_set_cfg() function. In order to set my system up to always have the AUX_P/N pins connected to SBU1/2, am I correct that I should be invoking it as:
retval = mux_ctrl_set_cfg (port, MUX_CONFIG_DP_4_LANE, dpm_get_polarity (port));
If so, where should this invocation take place? Should I be manually adding it to the initialization section of my main.c? If so, what value should I be passing in for the uint8_t port argument to mux_ctrl_set_cfg and dpm_get_polarity?
Are there any options in my config.h that I will need to disable to ensure that app_event_handler won't overwrite the mux settings that I give via my invocation to mux_ctrl_set_cfg when a new connection is detected? Or will I need to make any direct modifications to app_event_handler to ensure that my mux config isn't overwritten?
Thank you for your response.

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi,
As you have pointed out, mux_ctrl_set_cfg() is in turn called by set_mux() function. This set_mux() function is used to configure the mux at multiple places.
You can disable mux control by changing the MUX_TYPE macro present in solution.h to value other than DP_MUX. This will disable the control of this message through all parts of code.
>> For port value, you can use this macro - TYPEC_PORT_0_IDX
If so, where should this invocation take place? Should I be manually adding it to the initialization section of my main.c?
>> Yes
Pranava