Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB EZ-PD™ Type-C

td83
Level 1
10 questions asked 10 sign-ins 5 replies posted
Level 1

Hi,

On our board we are using the device CYPD5225 with a Tiger Lake.

The Tiger Lake supports DP++ Display over Type-C ports.

In DisplayPort mode the bus AUX+/- is connected to the SBU1/2 pin

In HDMI mode the bus I2C SCL/SDA is connected to the SBU1/2 pin

Is it possible to MUX these two signal inside the device CYPD2525 with the balls AUX+_P1/AUX-P1 and the balls LSRX_P1/LSTX_P1 ?

Thank you for help,

Best regards

TD83

0 Likes
1 Solution
PranavaYN
Moderator
Moderator 50 likes received First comment on KBA First question asked
Moderator

Hi,

There is an internal SBU MUX in CCG5 that can switch between LSTx/LSRx and DP_AUX_P/DP_AUX_N. Please refer to the figure below.

PranavaYN_0-1637062355474.png

You can use this internal MUX to switch between 2 signals. Please refer to SBU MUX section (Page 5) in the datasheet. https://www.cypress.com/file/363396/download 

Please let me know if you need any clarification regarding this.

Best regards,
Pranava

View solution in original post

0 Likes
1 Reply
PranavaYN
Moderator
Moderator 50 likes received First comment on KBA First question asked
Moderator

Hi,

There is an internal SBU MUX in CCG5 that can switch between LSTx/LSRx and DP_AUX_P/DP_AUX_N. Please refer to the figure below.

PranavaYN_0-1637062355474.png

You can use this internal MUX to switch between 2 signals. Please refer to SBU MUX section (Page 5) in the datasheet. https://www.cypress.com/file/363396/download 

Please let me know if you need any clarification regarding this.

Best regards,
Pranava
0 Likes