Announcements
IMPORTANT: Cypress Developer Community currently doesn’t allow sign-in to prepare for the upcoming transition. To learn more, check out our announcement.
cancel
Showing results for 
Search instead for 
Did you mean: 

USB EZ-PD Type-C

td83
New Contributor II

Hello,

I am looking for the tool to configure the device CYPD5225.

I have downloaded the software PSoC Creator 4.4, but i was not able to find the component CYPD5225 in this tool !

What is the tool to configure the registers on the CYPD5225 ?

What is the tool to generate the HEX file mention in the document "CCGx (CYPDxxxx) Programming Specifications" Document Number: 002-22328 Rev. *G ?

I have the tool to download the HEX file to the CYPD5225 device but not the tool to generate the HEX file.

Thank you for help,

Best regards,

td83

0 Likes
1 Solution
ShifangZ_26
Moderator
Moderator

Hello td83,

 

1. You can select read from firmware file to get configurations of the binaries, and then review/change the configurations via Ez-PD configuration Utility. But, you need a .hex or .cyacd file which is matching the hardware design you are working on. 

2. You could get .hex/.cyacd from the folder if you have been installed any SDK or Kit from www.cypress.com

For example, CCG5 hex files:

...(installed path)\Cypress\EZ-PD CCGx Host SDK\CCGx\Firmware\binaries

ShifangZ_26_0-1623803627355.png

 

3. If your hardware design is not match our reference design/Applications hardware on Datasheet, you have to generated .hex/.cyacd files by PSoC Creator based on example codes have been offered in SDK. And Ez-PD configuration Utility will generated .c file for your project and then you could replace config.c in PSoC Creator directly.

Best Regards,

Lisa

View solution in original post

0 Likes
3 Replies
ShifangZ_26
Moderator
Moderator

Hello ,

 

You need download the SDK of CCGx Host, download link: https://www.cypress.com/documentation/software-and-drivers/ez-pd-host-software-development-kit 

 

Best Regards,

Lisa

0 Likes
td83
New Contributor II

Hello Lisa,

Thank you for help.

With the software "ED-PD Configuration Utility" i have found the CYPD5225 device.

I tried to configured the device, but the generated format files differs from the format needed the the "PSoC Programmer" tool.

The software "EZ-PD Configuration Utility" does not support the "Miniprog3" !

With the software "EZ-PD Configuration Utility" i tried to save my configuration into a .hex format file with the menu File ==> Save to Firmware File.

But the tool asks to "READ" a ".hex" file and does not "WRITE" a ".hex" file !

How can i "convert" into a ".hex" format a configuration file generated with the tool "ED-PD Configuration Utility" ?

Thank you for help,

Best Regards,

td83

0 Likes
ShifangZ_26
Moderator
Moderator

Hello td83,

 

1. You can select read from firmware file to get configurations of the binaries, and then review/change the configurations via Ez-PD configuration Utility. But, you need a .hex or .cyacd file which is matching the hardware design you are working on. 

2. You could get .hex/.cyacd from the folder if you have been installed any SDK or Kit from www.cypress.com

For example, CCG5 hex files:

...(installed path)\Cypress\EZ-PD CCGx Host SDK\CCGx\Firmware\binaries

ShifangZ_26_0-1623803627355.png

 

3. If your hardware design is not match our reference design/Applications hardware on Datasheet, you have to generated .hex/.cyacd files by PSoC Creator based on example codes have been offered in SDK. And Ez-PD configuration Utility will generated .c file for your project and then you could replace config.c in PSoC Creator directly.

Best Regards,

Lisa

View solution in original post

0 Likes