cancel
Showing results for 
Search instead for 
Did you mean: 

USB EZ-PD™ Type-C

PaRi_1293246
New Contributor II

Hello,

Is the EZ-PD Configuration Utility available for the CYPD3125 (notebook port controller)?

Thank you

Best Regards,

Patrice

0 Likes
1 Solution
Sananya_14
Moderator
Moderator

Hello Patrice,

If you could wire the I2C pins to a connector, and add a USB-Serial device (CY7C65215) between your processor and the I2C connector, then you could directly test the EZ-PD Configuration Utility. You could also use the USB-Serial device on the CY4531 EVK and connect the I2C pins from J6 header on the daughter card to the CCG3 on your board.

No, the EZ-PD Configuration Utility is meant for I2C programming while the SWD programming is done through PSoC Programmer using MiniProg3/4. Please refer to the KBA for more details- CCGx Programming Methods - KBA97271

I would recommend buying the latest MiniProg4 programmer, although both of them are compatible with CCG3.

Best Regards,

Sananya

View solution in original post

0 Likes
18 Replies