Feb 08, 2021
08:40 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Feb 08, 2021
08:40 PM
Hi,
I am evaluating CY6611 EZ-USB HX3PD for a particular application that requires integration of a usb hub, USB PD and controller circuit for a peripheral device (servo).
The idea is to have a single USB wire for connection to PC and eliminate the need for external power adaptor or power supply.
Is this possible with CY6611 EZ-USB HX3PD?
Does it work without 19V external supply?
Can we use US port on CY6611 as a sink to power the USB hub and also supply 12V for the peripheral circuit (more specifically servo)?
Thanks,
Nilufar
Labels
- Labels:
-
ispn:39584:1:0
-
l1:314:1:0
-
USBEZ-PDType-C
1 Reply
Feb 10, 2021
11:12 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Feb 10, 2021
11:12 PM
Please check the details in the following thread
Re: CY6611 EZ-USB HX3PD as a PD sink - Cypress Developer Community