- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Following setps was testing :
1. BCR connect to Type C adapter and DC out connected two in series 100w5R
When changing sw1 the dc out doesn't change
2. BCR connect to CY4532 evk (main board type c connector) with PB application
DC out connected two in series 100w5R
Also not change in mesurment v and a. Via PB application add uart and request v and a
Voltage = pd_hal_measure_vbus(0);
Current = pd_hal_measure_vbus_cur(0);
I terminal on PC I see only voltage 5 and current is zero although I change the sw1 and we have load
Q: do I need update fw of BCR
Q: what I need to do in order to see changes on DCout onBCR board
Q: do I need change registers or any other changes on EZ-PD™ BCR HPI Utility
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
Thanks for the update. While running the noboot project in Debug mode, please ensure that the CCG_TYPE_A_PORT_ENABLE macro is disabled in stack_params.h and you have disabled the TypeA page in the schematic. Please go to the System tab in your DWR file and check if the Debug Select is set to SWD.
If you are using the CY4532 EVK, kindly check if jumpers J6, J7, J9 on the power board are open i.e. SWD lines are free for debugging.
Best Regards,
Sananya