- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
on main board DEBUG CONNECTOR ( J8 ) P1.0 is Pin 1: GPIO_1Unused GPIO. Tri-stated. Available for user customization
Potentiometer | CY4532 EVK | |
VCC | TP2/TP4 | VCC |
GND | TP16 | GND |
OUTPUT | P1.0 | OUTPUT |
in Cypress EZ-PD™ CCGx Power SDK User Guide.pdf Table 4: PSOC Creator Components :
in other hand says in the same document
in datasheet of CYPD3171
in PSoC creator example project CCG3PA Power Adapter with Direct Feedback Control no ADC sigma
Q: how how use ADC unit in order read potentiometer values i dont see any ADC deltasegma or SAR component ? how to use AMUX if specificly forbiden in this application see above ?
Solved! Go to Solution.
- Tags:
- ccg3
- delsig adc
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
Can you please try out the following things:
1). Use pd_adc_calibrate API before sampling the values.
2). Use the potentiometer measurement function in app_task() or main() instead of calling it in the led_timer_callback()
3) Try using AMUXB instead of AMUXA since it might be already in use for VBUS measurement.
Regards,
Mallika
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
The ADC component is not available in the PSoC Creator.
Both ADC and AMUX are handled by the stack level functions.
You can use the below function for accessing ADC:
uint8_t pd_adc_sample ( uint8_t port, PD_ADC_ID_T adc_id, PD_ADC_INPUT_T input )
This function will handle both AMUX and ADC at the lower level. The argument adc_id selects one of the 2 ADC's.
CCG3PA has 2 ADCs: ADC_0 and ADC_1. ADC_O is used for VBUS measurement and ADC_1 is available for customization. Please make sure to use the correct ADC for your design.
Best Regards,
Mallika
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
OK , so could use uint8_t pd_adc_sample ( uint8_t port, PD_ADC_ID_T adc_id, PD_ADC_INPUT_T input )
Q: port param in pd_adc_sample what is the meaning or purpose ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
The port argument in pd_adc_sample is simply for determining the port in case of dual ports.
However, since CCG3PA is a single port device, you can set it's value to 0.
Regards,
Mallika
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
HW connection
Potentiometer | CY4532 EVK | |
VCC | TP2/TP4 | VCC |
GND | TP16 | GND |
OUTPUT | j8 debuger connctor -> P2.1 | OUTPUT |
see link of Potentiometer https://www.waveshare.com/wiki/Analog_Test_Board
in adc_measurment.txt you see implement Potentiometer_Measurement_init, Potentiometer_Measurement_Print_Value
Potentiometer_Measurement_init() in main.c
Potentiometer_Measurement_Print_Value(0) calling in
void led_timer_cb (uint8_t port,timer_id_t id) the led is blinking properly each 100 ms
{
(void)port;
(void)id;
adc_system_measurment_t res;
res=Potentiometer_Measurement_Print_Value(0);
USER_LED_Write(!USER_LED_Read());
timer_start (0, LED_TIMER_ID, LED_TIMER_PERIOD, led_timer_cb);
}
but the measurement is not stable and not accurate see UART teraterm log attached
Q: what is accuracy of ADC 8 bit 10 bit or 12 bit ?
Q: why need convert to gpio in the end of calculation hsiom_set_config (GPIO_PORT2_PIN0, HSIOM_MODE_GPIO);
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
Q: what is accuracy of ADC 8 bit 10 bit or 12 bit ?
>> On the chip, 8 bit SAR ADC is available.
For more information please go through Table 39 (Page 28) in the CCG3PA datasheet https://www.cypress.com/file/363381/download.
Q: why need convert to gpio in the end of calculation hsiom_set_config (GPIO_PORT2_PIN0, HSIOM_MODE_GPIO)
>> It is necessary to free the AMUX (it should not be in use) so that the AMUX can then be accessed by the other gpios as well as to release the gpio from muxing and use it for other purposes.
This is done by changing the the HSIOM for that IO to HSIOM_MODE_GPIO.
Regards,
Mallika
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
in my application i need measurement simultaneously 3 GPIO which each of them is representing voltage and current measurement in period 100 ms
any advice ? how to approach this issue ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
Can you please further elaborate on your design and the functionalities you want to use so that we can better understand the issue and help you.
Regards,
Mallika
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
in my design of CYPD3175 i have tree GPIO
p1.0 -> Current Measurment
p1.1 -> Current Refernce
p2.2 -> Channel Address ( connected to resistor )
all this pin i need measurement ADC and get ADC digital level and Voltage
all this data i need for control in my application simultaneously and continuously
i tried connect Potentiometer to one of the legs t want recieve digital level and voltage of the Potentiometer is 1k so if ADC is 8 bit so in full range i need get 256 units but i get random numbers when print to UART Volatge values and digital level ( attched uart log in teraterm )
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
1. Are you working on only the main board (you have removed the power board) or is the power board there?
2. Can you please share your PSoC project?
Regards,
Mallika
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
Hello,
Can you please try out the following things:
1). Use pd_adc_calibrate API before sampling the values.
2). Use the potentiometer measurement function in app_task() or main() instead of calling it in the led_timer_callback()
3) Try using AMUXB instead of AMUXA since it might be already in use for VBUS measurement.
Regards,
Mallika
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
?what is max voltage to ADC 256 bit ( 8 bit adc ) ?