Announcements

Live Webinar: USB-C adoption. Simple & Cost-efficient solutions | April 18th @9am or 5pm CEST. Register now !

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Ivan_Lee
Level 5
Level 5
Distributor - Zenitron(GC)
100 replies posted 5 likes given 100 sign-ins

 

1. Does "VBAT to GND protection" and "VBUS OCP" use the same - resistor current sensor to detect  current ? ( pin#18 and pin#19)

2.  Application note : This resistor senses the current, and if it exceeds the firmware-configured threshold, the NFET is
turned off to interrupt the current. This protects against over-current conditions caused by external faults

How to set "VBAT to GND" firmware-configured threshold to different value ?

0 Likes
1 Solution
Pranava_YN
Moderator
Moderator
Moderator
100 likes received 500 replies posted 250 solutions authored

Hi,

VBat to GND protection uses the low-side CSA pins that you have mentioned. VBus OCP uses a high-side current sense resistor. They are 2 separate resistors. You can refer to the Application diagram present in the datasheet for this.

Regarding the threshold configuration, please refer to pd_internal_vbat_gnd_scp_level_set() API in the source code. This is used to change threshold value.

VBUS UVP is detected from VBUS_C pin which is connected to the VBUS of the Type-C Connector.

Best regards,
Pranava

View solution in original post

0 Likes
3 Replies
Ivan_Lee
Level 5
Level 5
Distributor - Zenitron(GC)
100 replies posted 5 likes given 100 sign-ins

Sorry i have another question which pin is used for detection UVP?

0 Likes
Roy_Liu
Moderator
Moderator
Moderator
5 comments on KBA First comment on KBA 10 questions asked

You may start a new thread if this is still an open question.😊

Roy Liu
0 Likes
Pranava_YN
Moderator
Moderator
Moderator
100 likes received 500 replies posted 250 solutions authored

Hi,

VBat to GND protection uses the low-side CSA pins that you have mentioned. VBus OCP uses a high-side current sense resistor. They are 2 separate resistors. You can refer to the Application diagram present in the datasheet for this.

Regarding the threshold configuration, please refer to pd_internal_vbat_gnd_scp_level_set() API in the source code. This is used to change threshold value.

VBUS UVP is detected from VBUS_C pin which is connected to the VBUS of the Type-C Connector.

Best regards,
Pranava
0 Likes