Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB EZ-PD™ Type-C Forum Discussions

julius_yang
Level 1
5 questions asked 5 replies posted 10 sign-ins
Level 1

1. CCG5平台UVP已经关闭,CCG5平台内部机制,会检测VBUS电压,当VUBS电压低于一定门限,会disconnect port吗?谢谢

2. 5V/3A, 9V/2A, 12V/1.5A, 15V/1.2A低压测试结果如下

    5V/3A: when VBUS decrease to 4V, will disable port,and trigger APP_EVT_DISCONNECT enent

    9V/2A:when VBUS decrease to 7.2V, will disable port,and trigger APP_EVT_DISCONNECT enent

    12V/1.5A:when VBUS decrease to 9.5V, will disable port,and trigger APP_EVT_DISCONNECT enent

    15V/1.2A:when VBUS decrease to 712V, will disable port,and trigger APP_EVT_DISCONNECT enent

3. 9V/2A与15V/1.2A测试uart、PD log如附件所示

    

julius_yang_0-1664206645177.pngjulius_yang_1-1664206650892.png

 

0 Likes
2 Replies
ShifangZ_26
Moderator
Moderator 250 sign-ins 1000 replies posted 750 replies posted
Moderator

Hello ,

请问是否可以提供您测试事件的完整log?(最好是txt格式。)

 

Best Regards,

Lisa

0 Likes
julius_yang
Level 1
5 questions asked 5 replies posted 10 sign-ins
Level 1

不要意思,忘了贴了,uart和PD log,请帮忙分析下,谢谢

0 Likes