九月 26, 2022
08:38 AM
1. CCG5平台UVP已经关闭,CCG5平台内部机制,会检测VBUS电压,当VUBS电压低于一定门限,会disconnect port吗?谢谢
2. 5V/3A, 9V/2A, 12V/1.5A, 15V/1.2A低压测试结果如下
5V/3A: when VBUS decrease to 4V, will disable port,and trigger APP_EVT_DISCONNECT enent
9V/2A:when VBUS decrease to 7.2V, will disable port,and trigger APP_EVT_DISCONNECT enent
12V/1.5A:when VBUS decrease to 9.5V, will disable port,and trigger APP_EVT_DISCONNECT enent
15V/1.2A:when VBUS decrease to 712V, will disable port,and trigger APP_EVT_DISCONNECT enent
3. 9V/2A与15V/1.2A测试uart、PD log如附件所示
2 回复数
九月 27, 2022
01:26 AM
Hello ,
请问是否可以提供您测试事件的完整log?(最好是txt格式。)
Best Regards,
Lisa
Attachments are accessible only for community members.
九月 27, 2022
02:03 AM