Announcements

Learn how to optimise USB-C for your designs at 18 May's USB-C PD Webinar.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

chch_3621411
Level 4
Level 4
First like given

Hello i'm using 2 CCG3PA in my system for a power bank one port will be dual role and the other will be source only, so i would like to connect them to communicate trough, I2C.

where should i put the i2c code in main ?
where should i put the code for checking the port role for example i would like to check if the port is sourcing power then blink blue led or if it is sinking power blink red led, where should i put the API code ?
for the led there's led only in main.c

#if APP_FW_LED_ENABLE

/* Blink the LED every LED_TIMER_PERIOD ms. This serves as an indication of the firmware running. */

void led_timer_cb (

    uint8_t port,

    timer_id_t id)

{

    (void)port;

    (void)id;

    gpio_set_value (FW_LED_GPIO_PORT_PIN, !(gpio_read_value (FW_LED_GPIO_PORT_PIN)));

    timer_start (0, LED_TIMER_ID, LED_TIMER_PERIOD, led_timer_cb);

}

#endif /* APP_FW_LED_ENABLE */

and in config.h there is this code for the led

* Enable/Disable firmware active LED operation.

*

* The blinking LED is enabled by default but it is recommended to disable it

* for production designs to save power.

*/

#define APP_FW_LED_ENABLE                           (0u)

/* Enable Internal UVP Comparator to be used as VBUS divider. */

#define VBUS_MON_INTERNAL                           (1u)

/*

* Select CCG3 GPIO to be used as Activity Indication. This should be set to a

* valid value if APP_FW_LED_ENABLE is non-zero.

*/

#define FW_LED_GPIO_PORT_PIN                        (GPIO_PORT_2_PIN_0)

/*

* Timer ID allocation for various solution soft timers.

*/

/*

* Activity indicator LED timer. The timer is used to indicate that the firmware

* is functional. The feature is controlled by APP_FW_LED_ENABLE.

*/

#define LED_TIMER_ID                                (0xC0)

/*

* The LED toggle period.

*/

#define LED_TIMER_PERIOD                            (1000)

1 Solution
ShifangZ_26
Moderator
Moderator
Moderator
10 likes given 250 sign-ins 1000 replies posted

Hi ,

For your questions,

1. where should i put the i2c code in main ?

>> You need add I2C initial in main() and before while(1).  And then, you could add others operations in app.c and call it in function void ccg_app_task(uint8_t port).

2. where should i put the code for checking the port role for example i would like to check if the port is sourcing power then blink blue led or if it is sinking power blink red led, where should i put the API code ?

>> You could add it into void ccg_app_task(uint8_t port).

And use below way to check whether it is source or sink.

Is it SOURCE?  >> dpm_get_info(TYPEC_PORT_0_IDX)->cur_port_role == PRT_ROLE_SOURCE

Is it SINK?  >> dpm_get_info(TYPEC_PORT_0_IDX)->cur_port_role == PRT_ROLE_SINK

Best Regards,

Lisa

View solution in original post

3 Replies
ShifangZ_26
Moderator
Moderator
Moderator
10 likes given 250 sign-ins 1000 replies posted

Hi ,

For your questions,

1. where should i put the i2c code in main ?

>> You need add I2C initial in main() and before while(1).  And then, you could add others operations in app.c and call it in function void ccg_app_task(uint8_t port).

2. where should i put the code for checking the port role for example i would like to check if the port is sourcing power then blink blue led or if it is sinking power blink red led, where should i put the API code ?

>> You could add it into void ccg_app_task(uint8_t port).

And use below way to check whether it is source or sink.

Is it SOURCE?  >> dpm_get_info(TYPEC_PORT_0_IDX)->cur_port_role == PRT_ROLE_SOURCE

Is it SINK?  >> dpm_get_info(TYPEC_PORT_0_IDX)->cur_port_role == PRT_ROLE_SINK

Best Regards,

Lisa

hello thanks for the answer,

so i have added

void ccg_app_task(uint8_t port)

{

    /*port role check API added on 04/07/2019*/

    dpm_get_info (TYPEC_PORT_0_IDX)->cur_port_role=PRT_ROLE_SOURCE;

    dpm_get_info (TYPEC_PORT_0_IDX)->cur_port_role=PRT_ROLE_SINK;

#if CCG_CABLE_COMP_ENABLE

in app.c batt i have error "cannot assing to return value because fucntion dpm_get_info can't return const value"

for the two API line

0 Likes

You should use comparison operator == instead of assignment operator =

Regards,

Muthu

0 Likes