Announcements

Live Webinar: USB-C adoption. Simple & Cost-efficient solutions | April 18th @9am or 5pm CEST. Register now !

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
KeTa_1341526
Level 5
Level 5
Distributor - TED (Japan)
10 likes given 10 likes received 5 likes given

Hello,

Use CCG2 with your Cable application.

It does not reset with XRES.

If you check the [Application Diagrams] in the data sheet, a 4.7kohm pullup is connected when XRES is not in use.

Is there no internal pullup in XRES?

If it exists, will it become a parallel resistor and weaken if 4.7kohm is connected?

Please tell me the correct connection method.

Best regards,

Takahashi

0 Likes
1 Solution
Sananya_14
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hi Takahashi-san,

Yes, the XRES pin is pulled high internally. 4.7k is our characterized value for external pull up on the XRES pin and will not weaken the overall resistance such that the device goes into reset. Please refer to the App Note for more details- https://www.cypress.com/file/151561/download

Best Regards,
Sananya

View solution in original post

0 Likes
6 Replies
Sananya_14
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hi Takahashi-san,

Yes, the XRES pin is pulled high internally. 4.7k is our characterized value for external pull up on the XRES pin and will not weaken the overall resistance such that the device goes into reset. Please refer to the App Note for more details- https://www.cypress.com/file/151561/download

Best Regards,
Sananya

0 Likes
KeTa_1341526
Level 5
Level 5
Distributor - TED (Japan)
10 likes given 10 likes received 5 likes given

Hi Sananya-san,

Thank you for your reply.

Can XRES be directly connected to VDDIO without the pull-up resistor?

Best regards

0 Likes

Hi Takahashi-san,

We recommend using a pull-up resistor to connect XRES to VDDIO and hence the datasheet application diagrams also include 4.7k pull-up on the pin.

Best Regards,
Sananya

0 Likes
KeTa_1341526
Level 5
Level 5
Distributor - TED (Japan)
10 likes given 10 likes received 5 likes given

Hi Sananya-san,

If VDDIO is directly connected, a large current will flow in and the current consumption will increase.

To prevent that, it's not directly connected to VDDIO (connected pullup:4.7kohm), right?

The value of the internal resistance of XRES is RPULLUP (8.5kohm to 3.5kohm), so if you connect a 4.7kohm pullup resistor to the outside, it is predicted that it will be about 2kohm to 3kohm.

Is the above recognition all right?

Best regards

0 Likes
KeTa_1341526
Level 5
Level 5
Distributor - TED (Japan)
10 likes given 10 likes received 5 likes given

Hi Sananya-san,

> If VDDIO is directly connected, a large current will flow in and the current consumption will increase.

Another reason is that it is easily affected by power supply noise, isn't it?

Best regards

0 Likes

Hi Takahashi-san,

Yes, your understanding is correct. However, I would have to check internally regarding the exact Rpullup range for XRES pin, although I think it should be similar to that for other GPIOs.

We also recommend connecting a decoupling capacitor of 0.1uF on the pin to avoid supply noise.

Best Regards,
Sananya

0 Likes