cancel
Showing results for 
Search instead for 
Did you mean: 

USB EZ-PD™ Type-C

NoAr_1540581
New Contributor II

We are considering demo with the following system configuration with CY4532 kit (power sink).
-  we do not need data tranfer.In a
[Syetem]  Note PC⇒CY4532 Main board (Type-C I/F) ⇒ Main board (type-A I/F) ⇒ Mobile phone

In addition,  we want to operate the PPS demo, too.

Q1) Is it possible to operate above system using CYPD3171-24LQXQ_cla_3_3_0_1882_0_0_0_pa.cyacd?
Q2) Could you please tell me if there is a sample FW that can output power to Type-A via Type-C on the main board?

Best Regards

Arai

0 Likes
1 Solution
HirotakaT_91
Moderator
Moderator

Hi Arai-san,

A1)

By default, CYPD3171-24LQXQ_cla_3_3_0_1882_0_0_0_pa.cyacd (FW) works only as Power Adapter (PA) or Power Bank (PB).

A2)

So far, there is no such a sample code.

If you are considering some demo by yourself, kindly contact Local Cypress FAEs or an appropriate Business Unit if you want to any help.

Best regards,

Hirotaka Takayama

View solution in original post

0 Likes
2 Replies
HirotakaT_91
Moderator
Moderator

Hi Arai-san,

A1)

By default, CYPD3171-24LQXQ_cla_3_3_0_1882_0_0_0_pa.cyacd (FW) works only as Power Adapter (PA) or Power Bank (PB).

A2)

So far, there is no such a sample code.

If you are considering some demo by yourself, kindly contact Local Cypress FAEs or an appropriate Business Unit if you want to any help.

Best regards,

Hirotaka Takayama

0 Likes
NoAr_1540581
New Contributor II

回答有難うございます

承知致しました

0 Likes