Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
alzh_1341656
Level 1
Level 1
Distributor - Future(GC)
First reply posted 10 sign-ins 5 sign-ins

Traveo II CYT4B can run on 350MHZ?      code is as follow:

#if (CY_SYS_PLL400M_0_FREQ == CY_SYS_PLL400M_0_350MHz)
// PLL_OUT = 24,000,000(Feco) / 3 * 125 / 5 = 200,000,000Hz
// Restriction: 400,000,000 <= Fvco <= 800,000,000
// This time, Fvco = 16,000,000 * 175 / 4 = 700,000,000.

#define CY_SYSTEM_PLL0_CONFIG_REFDIV (2UL)
#define CY_SYSTEM_PLL0_CONFIG_FEEDBACKDIV (175UL)
#define CY_SYSTEM_PLL0_CONFIG_OUTDIV (6UL)

/*
#define CY_SYSTEM_PLL0_CONFIG_REFDIV (3UL)
#define CY_SYSTEM_PLL0_CONFIG_FEEDBACKDIV (125UL)
#define CY_SYSTEM_PLL0_CONFIG_OUTDIV (5UL)
*/
#elif (CY_SYS_PLL400M_0_FREQ == CY_SYS_PLL400M_0_320MHz)

0 Likes
1 Solution
HongyanW_86
Moderator
Moderator
Moderator
100 solutions authored 100 replies posted 50 solutions authored

Hello,

According to Clock Diagram (Figure 7-1) or below table, CM7_0 is sourced from CLK_HF1, which is selected from PLL400#0 (out: 350MHz) in SDL 6.6 example (by default). Kindly review system_tviibh8m_cm0plus.c included in SDL and Chapter 18 of Clock System of Traveo II Body High Architecture TRM for more details.

//CYT4BF datasheet

HongyanW_86_0-1610934886144.png

Best regards,

Amy 

 

View solution in original post

0 Likes
2 Replies
Roy_Liu
Moderator
Moderator
Moderator
5 comments on KBA First comment on KBA 10 questions asked

Hi, 

This looks a questioning discussion, so it is moved from Code Example board to the current Traveo II board, this way the question could be caught by Traveo II community members faster.

P.S. Welcome to share your code(if any) as example with community members here when you want.

Roy Liu
0 Likes
HongyanW_86
Moderator
Moderator
Moderator
100 solutions authored 100 replies posted 50 solutions authored

Hello,

According to Clock Diagram (Figure 7-1) or below table, CM7_0 is sourced from CLK_HF1, which is selected from PLL400#0 (out: 350MHz) in SDL 6.6 example (by default). Kindly review system_tviibh8m_cm0plus.c included in SDL and Chapter 18 of Clock System of Traveo II Body High Architecture TRM for more details.

//CYT4BF datasheet

HongyanW_86_0-1610934886144.png

Best regards,

Amy 

 

0 Likes