TRAVEO™ T2G Forum Discussions
Hello Team,
I am LG India team,
we are using I2C driver provided by Infineon team to LG Korea team,
in I2C driver, Cy_SCB_I2C_SlaveGetReadTransferCount( ) is available which Returns the number of bytes read by the slave since the last time Cy_SCB_I2C_SlaveConfigReadBuf() is called.
we calling this function before Cy_SCB_I2C_SlaveConfigReadBuf().
but we found its not reading correct values.
could you test once share procedure to use.
We are looking for an MPU socket with below part number to use on a customer's prototype board.
・CYT4BFBDJS (272pin BGA)
Could you please tell me the supported socket part number of this MCU?
Thank you & Best regards,
顧客の試作基板上で使用するための、下記型番のMPUソケットを探しています。
・CYT4BFBxJSに (272pin BGA)
このMCUに対応するソケットの型番を教えて頂けますでしょうか?
よろしくお願い致します。
Show LessHello, everybody:
I encountered the following problem, read the value in the register, check the register is "0x80000e23", but after reading, the first bit is not read, only read "0xe23", the type of the variable used to receive the value of the register is ( volatile uint32 )
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/TRAVEO-T2G/%E8%AF%BB%E5%8F%96%E5%AF%84%E5%AD%98%E6%9C%BA%E7%9A%84%E5%80%BC-%E7%AC%AC%E4%B8%80%E4%B8%AAbit%E8%AF%BB%E5%8F%96%E4%B8%8D%E5%88%B0/td-p/743090
Show LessDoes modustoolbox support CMSIS-DAP for debugging TRAVEO II, and if so, how do I set it up?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/TRAVEO-T2G/modustoolbox-%E6%98%AF%E5%90%A6%E6%94%AF%E6%8C%81DAP/td-p/741605
Show LessHi,
I want to know CYT2B75CAE this controller is supporting AUTOSAR, If yes where i will get those information,
when i browse i am not able to find the information
Show Less你好!
在NORMAL状态下,我用WriteRow写NAR时报0xF00000AA(Writes are disabled in safety register)错误,
请问是什么原因?另外,可否提供使用WriteRow的例程?谢谢!
补充一点:这部分代码我是放在CM4里的,这可以吗?
Show LessDears
Please review my questions about secure booting as the following and give me your opinion.
(1) I'm wondering that how to see current life cycle stage of Traveo II MCU ?
(2) After successful secure booting, how to get the result of successful secure booting ?
Best regards,
Wonjin.
Show LessHello Experts,
I am referring this document (page 36) for my configuration of UART to 115200 baudrate. I am not getting desired output on my putty terminal(I can see continuous junk getting displayed)
FYI.. This is my Cy_SysClk_PeriphSetFracDivider function settings.
CLK_PERI Frequency external crystal = 20MHz
115200(baud rate) * 16(OVS) = Input Clock = 1843200 Hz
DIV24.5 = 20MHz / 1843200 = 10.8506
Fractional Divider
Integer : 10 , Fractional : 27 (0.8437 = 27/32)
I have one basic doubt is CLK_PERI freq is same as external crystal oscil(ECO)
Show Less您好,
请问当调用SDL的__NVIC_SystemReset函数(core_cm4.h)时CM0+和CM4核会都被reset吗?