TRAVEO™ T2G Forum Discussions
Dears
Please review my questions about secure booting as the following and give me your opinion.
(1) I'm wondering that how to see current life cycle stage of Traveo II MCU ?
(2) After successful secure booting, how to get the result of successful secure booting ?
Best regards,
Wonjin.
Show Less您好,
请问当调用SDL的__NVIC_SystemReset函数(core_cm4.h)时CM0+和CM4核会都被reset吗?
你好!
我的应用程序需要根据条件随时enable or diable DAP。
根据手册的说明,在生命周期为NORMAL_PROVISIONED时可以update normal access restriction。我理解调用SROM API Library的WriteRow(opcode:0x05)可以实现diable access DAP,但是,我找不到擦除SFLASH的API,我没有办法再次用WriteRow实现enable DAP。但是在AN228680的第22页说可以re_enable DAP,请问如何实现这一点?
Show Less
Hi Team,
I'm currently working with the CTY4DN microcontroller.
I'm utilizing the Cy_GPIO_SetHSIOM(base, pinNum, hsiom) API, which requires passing the port number as an argument.
To obtain the port number, I'm using the Cy_GPIO_PortToAddr(uint32_t portNum)function.
However, after referring to the CTY4DN driver files, I couldn't find the expected functionality.
Could someone provide guidance on how to correctly obtain the port number?
Thank you.
Show LessHi Team,
I have a question regarding the availability of the cyhal layer for the CYT4DN microcontroller.
Can someone confirm if this microcontroller supports the cyhal layer?
If so, could you please provide the necessary cyhal layer files? Thank you.
Show Less
Hello.
Regarding 3DL After entering deepsleep, the MCU current is around 4mA when measured separately. Both cores executed Cy_SysPm_DeepSleep to confirm that the MCU entered DeepSleep. what could the high current be related to?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/TRAVEO-T2G/3DL-deepsleep-%E7%94%B5%E6%B5%81/td-p/724510
Show LessIs there currently a CYT4BF port of the freeRTOS SMP sample program? What do I need to pay attention to when porting.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/TRAVEO-T2G/CYT4BF%E7%B3%BB%E7%BB%9FMCU%E6%94%AF%E6%8C%81freeRTOS-SMP%E7%A7%BB%E6%A4%8D%E5%90%97/td-p/732013
Show LessIs there a priority process for the CAN ID of Traveo T2G's sample driver library?
The test results seem to have a priority process in CAN ID.
Please tell me where the related processing part is.
Hi,
I have a query regarding library files. Currently, I'm using the TRAVEO_T2G - CYT4BF Micro series.
- For this microcontroller, I generated the library using modus toolbox and it's working.
- Now, I need to change the micro to CYT4DN. So, will the CYT4BF library support this series or not?
Can you please provide your input?
Thanks & Regards,
Yuvaraj