TRAVEO™ T2G Forum Discussions
T2G_Sample_Driver_Library_7.8.0 \tviibe1m\src\examples\tcpwm\pwm_DT\
pwm_DT.pdf
Port is 6.0 , 6.1 .
But, in source file , Port is P3.5 P4.0
Is it right?
If it is wrong, please give me the right source?
When we configurate the LIN_TX as strong, the LIN bus spike error always occur before break part is send.
But we configurate the LIN_TX as pull-up, no LIN bus spike error.
We don't know why.
Show LessHi,
I'm facing an error while trying to write SFlash (TOC2 region) via Lauterbach....
Flash boot has set an error code CY_FB_ERROR_INVALID_APP_SIGN
Now am not able to erase/program code flash too....
Is it possible to recover the board from this error? If yes, please guide
Show LessI would like to use an external oscillator on my Traveo2 CYT2B64. Are there selection conditions other than Table 26-23 in the data sheet?
It use Murata's CSTNE10M0G55A000R0 and would like to know if it meets the requirements.
Thanks,
Tetsuo
Hello.
I'm using Traveo II CYT2B93x.
I download a total of three firmware files (HSM, FBL, APP) onto the CYT2B93x MCU using Miniprog4, where HSM file is downloaded to the CM0P core and FBL & APP file are downloaded to the CM4 core.
I understand that HSM firmware needs to be downloaded first, but could you explain the reason behind it?
In the case of other MCUs, downloading the HSM firmware first can cause problems, so they download the HSM firmware last. Is there no issue related to the download order of HSM firmware in Traveo II?
Thank you.
MSV.
Show Less
Dear
I used Microcontroller CYT2B7 80-LQFP , we use 3rd part software tool can't set SPI MOSI port Direction = PIN IN and Driver Mode = PORT_PIN_OUT_MODE_PULLUP(3rd part configuration tool can only generate Driver Mode = PORT_PIN_OUT_MODE_HIGHZ), if I set SPI MISO port with Direction = PIN_IN and Driver Mode = PORT_PIN_OUT_MODE_PULLUP by manual code whether CYT2B7 Microcontroller can work well?
Show LessI used Microcontroller CYT2B7 80-LQFP
1st, I use only SAR2 ADC group, ADC channel from 0 to 7 were used channel 7 is the last channel .
2nd, I get ADC convert result by copy PASS0_SAR2_CHx_RESULT register value not by interrupt and DMA.
3rd, I get ADC convert result timing is check register PASS_SAR_CH7_INTR_MASK bit0 GRP_DONE_MASK [0:0] set to 0x1.
My question is if we only check register PASS_SAR_CH7_INTR_MASK bit0 GRP_DONE_MASK [0:0] set to 0x1, Can I consider no ADC group and Channel overflow happened and don't need both check GRP_OVERFLOW_MASK[2:2] and CH_OVERFLOW_MASK[10:10]. Is the GRP_DONE_MASK and GRP_OVERFLOW_MASK are mutual exclusion.
Thank you to the answer.
Best regards
Show LessIn "19. Triggers One-to-One" of the data sheet, there is the following description.
Isn't PWM0_M_3 a typo for PWM0_M_1? Similarly, isn't PWM0_M_6 a typo for PWM0_M_2?
Thanks,
Tetsuo
請問Traveo 的HSM Public Key 如何燒錄到HSM. 是否要用特殊的tool + software 或是其他的做法?
The pin connections for using an external PMIC with a Traveo II CYT4BF MCU would depend on the specific model of the MCU and the PMIC you are using.
The Traveo II CYT4BF MCU's Fault System function can provide a signal when a fault occurs, but it's not clear, whether that signal can be connected directly to the Error Monitoring Pin of the Infineon TLF35584 or NXP FS26 PMIC.
It is recommended to consult the datasheets and reference manuals for both the Traveo II CYT4BF MCU and the Infineon TLF35584 or NXP FS26 PMIC to determine the correct pin connections. You may also want to consider reaching out to the manufacturer's technical support for further guidance on this matter.
Show Less