TRAVEO™ T2G Forum Discussions
1.需求: RGB888 TTL简单输出图片,不需要渲染。
2.调试现状:由于我公司原因无法买图像库,我在SDL的T2G_Sample_Driver_Library_7.3.0\tviic2d4m\src\mw\gfx_env,T2G_Sample_Driver_Library_7.3.0\tviic2d4m\src\examples\gfx_env目录中找到了相关的用例!
3.问题:贵公司官网找不到任何关于上述文件夹代码的Training,我只能看懂大概,但是图片数据如何推入显存!如何配置显存地址在该用例都没有找到!能否提供关于相关开发的文档说明!或者非图像库的开发流程!非常感谢!
Show Less您好:在做LIN slaver. 时 用的是例程。接收主机发送的数据。只有同步错误中断标志,始终不能正常接收。
Hi All,
Is there a location in eFuse where a encryption key is already blown in Traveo II Body High chips by Cypress?
or
We have to write the encryption keys in the Customer Data eFuse region?
When I went through the TRM I found that eFuse bit contains encryption keys under section 37.6 eFuse memory
But I couldn't find it in the section 11.4.2 eFuseBits.
Also could someone clarify what is the use of Device Key functionality in Cryptography Block.
If there are Device specific keys then in which memory these keys are stored?
Whether these keys are accessible outside of Secure region(HSM)?
Hello everyone,
Can someone share MiniProg4's Auto Flash Utility 1.4 version and it's user guide download link.
Hi
I'm considering using CYT3DL/CYT4DN.
I couldn't check for MIPI DSI in the MCU's datasheet.
However, I confirmed the MIPI CSI contents.
I checked the MIPI D-PHY content in CYT3DLABHBQ1AESGS at the link below.
Q : Does TRAVEO CYT3DL/CYT4DN support MIPI DSI?
Thank you.
MSV.
Show Less目前使用的IC为CYT3DLABHBQ1AESGS,SDL为T2G_Sample_Driver_Library_7.8.0,详细信息如下图,标出的三个工程有如下疑问,烦请帮忙解答,谢谢
Q1:tviic2d4m_flash_cm0plus_cm7_0_template.eww是否支持MO跳转到M7?
Q2:tviic2d4m_flash_cm0plus_template.eww是否仅仅适用于M0?
Q3:tviic2d4m_flash_cm7_0_mc_template.eww是否仅仅适用于M7?
Q4:tviic2d4m_flash_cm0plus_cm7_0_template.eww和tviic2d4m_flash_cm0plus_template.eww代码好像一样的,是否用tviic2d4m_flash_cm0plus_cm7_0_template.eww即可?
Show Less
Hi
Good Morning
Miniprog3 support the -M4F microcontroller TRAVEO™ T2G family, I currently use the Psoc Programmer version 3.29.5
Im appreciate it
Show Less