Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

TRAVEO™ T2G Forum Discussions

ee1
TRAVEO™ T2G
I found that in the CYT 4B CM0 core, the timer interrupt cannot be used to CPUIntIdx0_IRQn to the CPUIntIdx2_IRQn, otherwise the interrupt cannot be e... Show More
Bhagyalakshmi
TRAVEO™ T2G
i want to configure CANFD for 8MBPS baudrate could u please helpme out how to configure ? i have configured for 2mbps it was working fine.but not able... Show More
ee1
TRAVEO™ T2G
Hello, I need to trigger the ADC with TCPWM, the ADC is triggering the dma, transmitting 2048 points, and the sampling frequency is 8Khz. The problem ... Show More
nsmr143
TRAVEO™ T2G
Hello Infineon Team, I have read the below mentioned article and planning to use this design. In my project the port is having only 2 supported smar... Show More
ivan1979
TRAVEO™ T2G
Good day together, I´m new with Traveo. My scenario: 1) CM7_0 core started by CM_0+ core (working) 2) CM7_0 core to start CM7_1 (working) 3) CM7_0 cor... Show More
TM_ben_liu
TRAVEO™ T2G
When I was developing bootloader, the client needed to keep the erasure and writing of flash in the MCU safely. It was necessary to separate the erasu... Show More
GavinLi
TRAVEO™ T2G

Hi 贵司大牛,

想问一下,CTT4BF上的QSPI 最大读、写速度是多少?

我在用户手册以及datasheet上没有看到相关信息,是在什么地方我忽略了吗?

 

谢谢!

Gavin

Translation_Bot
TRAVEO™ T2G
I can't capture PWM with P13.4 and it gets stuck in this code   Show More
GavinLi
TRAVEO™ T2G

Hi 贵司的技术大牛,

想请教一下,如何开启/使用该芯片PLL 的展频功能?有什么详细的步骤或是相关case可以参考吗?

谢谢!

Gavin

Forum Information

TRAVEO™ T2G

Discussion forum regarding 32-bit TRAVEO™ T2G Microcontroller - based on ARM® for automotive body electronics applications; cutting-edge performance, safety, and security features topics.