Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

TRAVEO™ T2G Forum Discussions

Kang_Kevin
TRAVEO™ T2G
Hi, 我手上有CYTVII-B-H-8M-176开发板,用IAR 9.50.1 目前有一个需求,需要制作一个OTA功能的固件,它完成用flash刷写CM7的app固件。 从几个文档中了解到,做这种OTA功能可以用dual bank来完成。但目前我只要single bank就行了,所以我的想法是:在... Show More
PradeepCool
TRAVEO™ T2G

Hi All,

Is there any Free Running Timers with CYT2CL Traveo T2G Cluster Application?

Thanks,
Pradeep

Ankita1
TRAVEO™ T2G
I am using SPI Communication sending 128 Bytes of FIFO. Setting Source Frequency 80MHZ and SPI buardrate is 5MHZ. I want to check how much time requir... Show More
KaiOops
TRAVEO™ T2G

ADC引脚悬空时,串联在ADC引脚上的电阻有0.1V的分压,难道ADC悬空时,引脚不是高阻态?

taegyunahn
TRAVEO™ T2G
Hi I'm using CYT2B9. The UART line in HW consists of 1 Wire. So, UART communication is performed with the TX/RX pins shorted on the MCU. I couldn't fi... Show More
Kang_Kevin
TRAVEO™ T2G

你好,我新买了一块CYTVII-B-H-8M-176 CPU BOARD,芯片丝印是CYT4BF8CDDES,请问有关于这款芯片或这个系列的示例demo吗? 

另外,示例中是否有单独的bootloader工程呢?

感谢解答。

gslm
TRAVEO™ T2G
Hello!Our team was tasked with developing a HW boad for the CYT2BL5CAAQ0AZEGS automotive microcontroller. We need to do a basic peripheral bringup fir... Show More
oferorgal
TRAVEO™ T2G
Hello, Where can I fined Download TRAVEO T2G Sample driver Library version - 7.2.0 for download?   I can only find later versions. All the best, Ofer. Show More
Forum Information

TRAVEO™ T2G

Discussion forum regarding 32-bit TRAVEO™ T2G Microcontroller - based on ARM® for automotive body electronics applications; cutting-edge performance, safety, and security features topics.