Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

TRAVEO™ T2G Forum Discussions

taegyunahn
TRAVEO™ T2G
HiI am using CYT2B9 and CYT4BF series.   I have a question about SAR ADC Vmotor / ADC[x]_M.I was able to see “One channel is also reserved for motor s... Show More
PatrickPavle
TRAVEO™ T2G
Dear Community,  I would like to toggle the LED 1 (P.19.0) and LED 4 (P12.2) on my board. How I configure, initilaze the ports and pins in the source ... Show More
NXTY_Sekino
TRAVEO™ T2G
I am trying to run T2G_Sample_Driver_Library_7.9.0 using GHS MULTI and CYTVⅡ-B-E-100-SO. I have a question about the definition of CPU_BOARD_REV in tv... Show More
chandan1995
TRAVEO™ T2G
we are using ADC[1]_3 Pin P5.3. for adc reading . but not getting expected results. #define BB_POTI_ANALOG_MACRO PASS0_SAR0 we are using S... Show More
taegyunahn
TRAVEO™ T2G
Hi. I am using CYT4BFCCJ. And tested with CYTVII-B-H-8M-320-CPU and SDL v8.0.0(examples/scb/spi/High_level_driver/api)   After setting up the SPI mast... Show More
GavinLi
TRAVEO™ T2G
Hi 贵司技术大牛们, 从CYT4BF的datasheet上,看到: 是指对引脚的电流注入和抽取最大是10mA吗? 如果不是,那么引脚的电流注入和抽取电流最大是多少? BR, Gavin Show More
rbs2kor
TRAVEO™ T2G
Hi, We are working on a project using Traveo T2G CYT4BF and CPU utilization is very high. We have enabled Icache. 1. We wanted to understand how to op... Show More
Translation_Bot
TRAVEO™ T2G
When using the T2G4BB7 SDL library, I found that the TCPWM module has everything other than the example program for orthogonal decoding (figure below)... Show More
pillar611
TRAVEO™ T2G
我是新手才开始学习使用这个软件,我按照demo程序对环境进行设置先选择devices:Cypress CYT2B75CA_M0+,然后选择Debugger-drivers是CMSIS DAP,CMSIS DAP中setup-reset选的是disabled(no reset),interface选择... Show More
yefe
TRAVEO™ T2G
1. In dual blank, does NVM only need to be configured with a size of 64k (the total size of work Flash is 128k)2. Will the data written to workFlash t... Show More
Forum Information

TRAVEO™ T2G

Discussion forum regarding 32-bit TRAVEO™ T2G Microcontroller - based on ARM® for automotive body electronics applications; cutting-edge performance, safety, and security features topics.