Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

TRAVEO™ T2G Forum Discussions

lokesh0806
TRAVEO™ T2G
Hi, We are getting the SPI status busy API "Driver_SPI.GetStatus(SpiDrvDSRC);"for infinite loop, while we are sending command. This is sporadic issue ... Show More
Translation_Bot
TRAVEO™ T2G
#TC39XB Description of the problem: The section I set is a const type, 1. Set up a section, then add objects to this section, #define XXX_INFO __attri... Show More
bscis1986
TRAVEO™ T2G
CYT2B75
solved msg Solved
CYT2B75的手册中没有ADC详细的说明,每个ADC支持内部6个连接用于诊断和监测,文档没有看到详细的描述。 Show More
gihong
TRAVEO™ T2G
Hello, everyone. I want to use SCB Uart's Baudrate set to 2M. And I have questions like this. 1. When I use CTX/RTX Port, Is there a case where it nee... Show More
tony
TRAVEO™ T2G
The chip I am currently using is CYT2B75BADQ0AZEGS. Now I want to know the difference in the time it takes to read, erase, and write to Work Flash and... Show More
Jackson_hwang
TRAVEO™ T2G
The CANFD driver is provided in the TRAVEO T2G Sample Driver Library files. Is there also a Classic CAN driver files? T2G_Sample_Driver_Library_7.8.0\... Show More
WonjinHan
TRAVEO™ T2G
Dears.   Now I use event generator in CYT2B98CAS with evaluation board of CYTVII-B-E-176-SO. Event generator operation is working well. Whenever event... Show More
sangbiao123
TRAVEO™ T2G
hello, dear infineon engineer. recently i am using a evaluation board. the board info silk print like this : TVII-B-H-8M-320-BGA CPU 600-60569-01 REV ... Show More
taegyunahn
TRAVEO™ T2G
HiI am using CYT2B9 and CYT4BF series.   I have a question about SAR ADC Vmotor / ADC[x]_M.I was able to see “One channel is also reserved for motor s... Show More
PatrickPavle
TRAVEO™ T2G
Dear Community,  I would like to toggle the LED 1 (P.19.0) and LED 4 (P12.2) on my board. How I configure, initilaze the ports and pins in the source ... Show More
Forum Information

TRAVEO™ T2G

Discussion forum regarding 32-bit TRAVEO™ T2G Microcontroller - based on ARM® for automotive body electronics applications; cutting-edge performance, safety, and security features topics.