TRAVEO™ T2G Forum Discussions
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/TRAVEO-T2G/CYT2B73-%E4%BD%BF%E7%94%A8greenhills%E7%BC%96%E8%AF%91%E5%99%A8%E6%97%B6-%E6%97%A0%E6%B3%95%E5%B0%86%E6%95%B0%E7%BB%84%E5%90%8D%E5%BC%BA%E5%88%B6%E8%BD%AC%E6%8D%A2%E4%B8%BA%E5%87%BD%E6%95%B0%E6%8C%87%E9%92%88-%E5%BA%94%E5%A6%82%E4%BD%95%E8%A7%A3%E5%86%B3/td-p/687609
Show LessTo write data to flash on Traveo 2 processors, a sector erase must be performed first, but when performing a sector erase, a 32-bit address is cleared. Even if I wanted to print an 8-bit value, I would waste the life of the 32-bit address. For this reason, I want to use Flash EEPROM emulation. Is there a source file for this?
Show LessI found that in the CYT 4B CM0 core, the timer interrupt cannot be used to CPUIntIdx0_IRQn to the CPUIntIdx2_IRQn, otherwise the interrupt cannot be entered, please why
Show LessHello, I need to trigger the ADC with TCPWM, the ADC is triggering the dma, transmitting 2048 points, and the sampling frequency is 8Khz. The problem is that when DMA srcTxsize is set to 32bit, it originally took 266ms to collect 2048 points, but now it only takes 160ms, which is not normal, because I use a timer to sample at equal intervals, and when srcTxsize is set to 16bit, it is 266ms (I will change the number of bytes and datasize of the array accordingly), and I found that changing the division coefficient of the timer clock will cause DMA to not be transmitted. I suspect there's something wrong with the clock. Below is my system configuration code, and ADC, DMA, TCPWM configuration code.
Show LessGood day together,
I´m new with Traveo.
My scenario:
1) CM7_0 core started by CM_0+ core (working)
2) CM7_0 core to start CM7_1 (working)
3) CM7_0 core to stop CM7_1: here I need first to put CM7_1 to Sleep. Question: as far as I understood (acc. infineon example code) one way is to use IPC.
Is there any other alternative and more direct way to let a core send another core to sleep mode?
I´d like to avoid to use IPC infrastructure.
For example with Tricore one core can "easily" stop another core by directly manipulating the CSFR register of the core to be stopped.
Thanks in advance for any input.
Ivan
Show LessWhen I was developing bootloader, the client needed to keep the erasure and writing of flash in the MCU safely. It was necessary to separate the erasure and writing operations of flash to make flash driver. Each upgrade sends the flash driver through the host computer to the mCU to run in ROm. Now the problem is how to make flash driver?
Show LessHi 贵司大牛,
想问一下,CTT4BF上的QSPI 最大读、写速度是多少?
我在用户手册以及datasheet上没有看到相关信息,是在什么地方我忽略了吗?
谢谢!
Gavin