TRAVEO™ T2G Forum Discussions
Hi
I'm using CYT2B9.
The UART line in HW consists of 1 Wire. So, UART communication is performed with the TX/RX pins shorted on the MCU.
I couldn't find SCB UART Rx/Tx Enable or Disable in the datasheet or TRM.
Q) How to control UART Rx, Tx Enable, Disable?
Thank you. Best & Regards.
taegyunahn.
Show Less你好,我新买了一块CYTVII-B-H-8M-176 CPU BOARD,芯片丝印是CYT4BF8CDDES,请问有关于这款芯片或这个系列的示例demo吗?
另外,示例中是否有单独的bootloader工程呢?
感谢解答。
Hello!
Our team was tasked with developing a HW boad for the CYT2BL5CAAQ0AZEGS automotive microcontroller. We need to do a basic peripheral bringup firmware.
Since this would be just for HW validation, I am assuming I would not need the MCAL license, correct? I so, I would like to know which toolchain / IDE to use - since this is an automotive item, is there any cost to the development IDE? If not, where could I download it?
Also, is there any evaluation board / demo kit for this MCU line, or for a similar one?
Hello,
Where can I fined Download TRAVEO T2G Sample driver Library version - 7.2.0 for download?
I can only find later versions.
All the best,
Ofer.
Show Less
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/TRAVEO-T2G/CYT2B7-can-id-filter%E8%AE%BE%E7%BD%AE%E6%8C%87%E5%AE%9Aid-0x7A1-%E4%B8%8D%E8%83%BD%E8%AF%86%E5%88%AB-%E4%BD%86%E8%AE%BE%E7%BD%AE%E4%B8%BA0xA1%E5%8F%AF%E4%BB%A5%E6%AD%A3%E5%B8%B8%E8%AF%86%E5%88%AB-%E6%98%AF%E5%90%A6%E5%AF%B9id%E6%9C%89%E9%99%90%E5%88%B6-%E5%8E%9F%E5%9B%A0%E6%98%AF%E4%BB%80%E4%B9%88/td-p/685896
Show Less
The code is as follows, the DMA can't transfer data, but it enters the interrupt the moment it is triggered by the software, and it can't enter the interrupt again
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/TRAVEO-T2G/CYT4BB%E5%8D%95%E7%89%87%E6%9C%BADMA%E4%B8%8D%E8%83%BD%E4%BC%A0%E8%BE%93%E5%8D%B4%E5%BC%82%E5%B8%B8%E8%BF%9B%E5%85%A5DMA%E4%B8%AD%E6%96%AD/td-p/688790
Show LessThe ADC is triggered with tcpwm, the ADC triggers the dma. 2048 points are captured and transported into the interrupt. The time interval to enter the interrupt is about 250ms, the target array is 16 bits, and the datasize is 16 bits. If srcTxfrSize is set to 1, the time to enter interrupt will be shortened to 150ms. If I replace the ADC result register with a 16-bit array as the source array and set srcTxfrSize to 0, the time to enter interrupt will be 250ms, how to solve this problem? Thank you for your help.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/TRAVEO-T2G/cyt4bb-DMA%E4%BC%A0%E8%BE%93%E6%97%B6%E9%97%B4%E5%BC%82%E5%B8%B8/td-p/690170
Show Lesssmartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/TRAVEO-T2G/CYT2B73-%E4%BD%BF%E7%94%A8greenhills%E7%BC%96%E8%AF%91%E5%99%A8%E6%97%B6-%E6%97%A0%E6%B3%95%E5%B0%86%E6%95%B0%E7%BB%84%E5%90%8D%E5%BC%BA%E5%88%B6%E8%BD%AC%E6%8D%A2%E4%B8%BA%E5%87%BD%E6%95%B0%E6%8C%87%E9%92%88-%E5%BA%94%E5%A6%82%E4%BD%95%E8%A7%A3%E5%86%B3/td-p/687609
Show Less