hello,
I am trying to generate hex and elf file with cmakelists for blink led project.
I am also using IAR files from the traveo SDL folder tviibe1m.
Unfortunately, I am not able to create the hex and elf even the compilation is without errors.
Would appreciate if you can review my project.
thanks,
Show Less
Hello.
Is there the method to select specific miniprog4 in several miniprog4?
I saw the manual of the autoflash utility.
But, I can't find the method.
Please check it.
Thanks and Best regards.
Glenn.
Show LessHi,
Going thoroughly through CYT4BF datasheets and TRM, I see that the MCU has 2 M_TTCAN controller with 5 channels each. What are the limitations of such an arrangement? Typically, MCUs use a 1:1 mapping controller to channel.
Basically I'm looking to answer these questions:
1. Does this arrangement have any hidden limitations that are not clear?
2. Can all channels operate independently at a different bit rate at full CAN-FD capacity of 5Mbps at the same time (that is - all 5 channels connected to active peripherals operating full speed of 5Mbps at the same time)?
3. If there are shared functions that cause performance impacts, what are they?
Thank you for your support!
Vai
Show Less
Hi,
MCU CYT2B75
If the global for ADC unit settings "DIAG_EN" and "EPASS_MMIO.PASS_CTL.REFBUF_EN" are set for diagnostic purposes, are those settings affect on all ADC groups (channels). For example I want to use only two channels per unit for diagnostic purposes.
Best rgeards,
Show Less参考SDL7.3 :T2G_Sample_Driver_Library_7.3.0\tviibe1m\src\examples\flash\code\cm0_cm4_non_blocking 文件夹下示例验证non-blocking 操作flash;
有如下疑问,请帮忙解答:
在调用Cy_FlashInit时,虽然是初始化non-blocking模式,
但在后续Cy_FlashWriteCode()函数里,在调用Cy_Flash_ProgramRow之前初始化参数时,
programRowConfig.blocking仍是按blocking模式进行设置,那最终program还是blocking啊
这个地方为什么要做这样的配置呢?
另:TraveoII中Flash Macro的数量有多少呢?TRM手册或代码中都没有体现?
Show Less
Hi All,
Is there any way to measure CPU load based on task using miniprog4 debugger.
Hi ,
Good day.
I have a questions about read blank work flash through SWD.
I found there is different behavior while CYT2B7xx/CYT4BBxx series read blank work flash.
For CYT4BB/BL series : it is able to read out the random (spurious) data from work flash.
For CYT2B7/BL series : it is unable to read out the random data, and it always shows ACK fault of SWD.
I want to know it is possible to set up CYT2B7's register to make the behavior is same as CY4BB series?
in other words, I hope CYT2B7/BL is able to be read random data if work flash is blank.
Thank you.
Jack
Show Less
Hi ,
Is it possible to create a single hex file from two different srec files that can be used to to flash the Bank A and Bank B in a single command using miniprog ?
Regards
Gokul
Show LessHello,
I try AES 128 CBC in Demo Project is OK,
But after I move the code to my own Project, it will stop at Cy_Crypto_Enable,
When it is confirmed that it is Cy_Crypto_Enable, Cy_Crypto_Sync will be called, and Cy_Crypto_Sync has no result.
Of course, I followed the instructions to set Cy_Crypto_Server_Start and NVIC of CM0+,
Cy_Crypto_Init for CM4.
May I ask what circumstances will cause Cy_Crypto_Sync to have no results?
In addition to appending (libcrypto_client_cm4_ghs.a),(libcrypto_server_cm0plus_ghs.a) what else needs to be set in the project?
Hello,
I have the CYT4BB controller operating in dual bank mode, with the FOTA use cases implemented and working. Is it possible to flash the Bank A and Bank B with separate binaries using the miniprog directly rather than rely on FOTA ? The objective is to have a special self test firmware flashed to Bank B and normal operating firmware in Bank A and it can be switched based on specific diagnostic requests.
Thanks
Gokul
Show LessUser | Count |
---|---|
11 | |
3 | |
2 | |
1 | |
1 | |
1 |