Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

TRAVEO™ T2G Forum Discussions

MerrimanInd
TRAVEO™ T2G
Hello all, I'm trying to run the Rust GPIO example on the T2G Body Entry Starter Kit. I seem to have the toolchain set up correctly, the code compiles... Show More
sangbiao123
TRAVEO™ T2G
dear infineon engineer. i want to add the freertos code to the  TVII_Sample_Driver_Library_7.0.0 or lower version,  is there any manual to refer to. o... Show More
JQ
TRAVEO™ T2G
 use SDL V7.9    D:\T2G_Sample_Driver_Library_7.9.0\tviibh8m\src\examples\syspm\DeepSleep\Wakeup_From_GPIO_Interrupt   DEMO,    Using the B-H-8M board... Show More
Nithyanantham
TRAVEO™ T2G
I'm working on a project with CYT4BF8CDS Microcontroller In cypress Driver they have only Drive Mode not having Pin Mode. Is there any possible to ch... Show More
krishnawa
TRAVEO™ T2G
We are replacing the controller in our unit with CYT2CL7BAAQ0AZSGS. Before, it had an NXP-based controller called MC9S12XHZ512 with a dedicated pin fo... Show More
Translation_Bot
TRAVEO™ T2G
Hello! The MCU hibernation cannot be woken up if it is not switched to internal power supply before executing deepsleep. 1) Is power switching done by... Show More
RMartins84
TRAVEO™ T2G
Hello Everyone I need to use the flash tool Cypress AutoFlash Utility in order to program the CYT2B97CAS. Does someone have the installer  download  l... Show More
Translation_Bot
TRAVEO™ T2G
Hi, I'm using the CYTVII-B-H-8M-176 development board, IAR 9.50.1 Currently working on an OTA project, in the CM0+ project, after flash flashing and u... Show More
Nithyanandan
TRAVEO™ T2G
During debugging, "why PLL unlock register is toggling back and forth(1 & 0). ? Show More
taegyunahn
TRAVEO™ T2G
Hi I want to know the core power stabilization time when transitioning from DeepSleep to Active in CYT4BF. I checked the power mode transition times a... Show More
Forum Information

TRAVEO™ T2G

Discussion forum regarding 32-bit TRAVEO™ T2G Microcontroller - based on ARM® for automotive body electronics applications; cutting-edge performance, safety, and security features topics.