Nov 02, 2021
11:03 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Nov 02, 2021
11:03 AM
Looking at the CYT4BB clocking diagrams, the only > 1MHz clock option for the watchdogs (WDT, MCWDT) appears to be the ECO.
This is a problem for me, because I am using an oscillator with EXTCLK. The EXTCLK pin used however is 21.2, which is shared with the ECO.
Question: Is it supported to use ECO with an external (LVCMOS, 3.3V) oscillator rather than a crystal?
P21.3 is unconnected, so no concerns about load levels etc on that pin.
Labels
- Labels:
-
Automotive Traveo_II
1 Reply