Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
yuejin
Level 1
Level 1
First reply posted First question asked Welcome!

Hi!

I have a  problem。

In M4 Core ,I use Cy_Flash_BlankCheck to check the address,the function return CY_FLASH_DRV_FLASH_NOT_ERASED。But I read the address,it will go the hardfault。

code:

uint32_t  ReadWFlashU32 (uint32_t add)

{

    uint32_t ret;

    cy_stc_flash_blankcheck_config_t blankCheckConfig;

   blankCheckConfig.addrToBeChecked = (uint32_t*)add;
   blankCheckConfig.numOfWordsToBeChecked = 0x1u;

   if ( CY_FLASH_DRV_FLASH_NOT_ERASED == Cy_Flash_BlankCheck(NULL, &blankCheckConfig,    CY_FLASH_DRIVER_BLOCKING))

   {
        ret = (*(uint32_t *)add); 
   }

   else
   {
        ret = 0x00000000uL;
    }

    return (ret);

}

0 Likes
6 Replies
Kavya_B
Moderator
Moderator
Moderator
100 replies posted 10 likes given 25 solutions authored

Hello Tian,

 

It seems that BlankCheck SROM API which in turn gets invoked inside Cy_Flash_BlankCheck() is not successful and hence you are getting the error code (CY_FLASH_DRV_FLASH_NOT_ERASED - 0xF00000A4).

 

Is the work flash region for which you are trying to do blank check protected? Is there any access restrictions set in your project for this memory address?

 

Thanks,

Kavya

0 Likes
yuejin
Level 1
Level 1
First reply posted First question asked Welcome!

Hello Kavya,

How many cases will return (CY_FLASH_DRV_FLASH_NOT_ERASED - 0xF00000A4).

I read address is 0x14019de4 ,it is in the chip workflash range.

I do not setting any protected , unless it is the default. How can I know  this address is protected?

 

 

0 Likes
yanf
Moderator
Moderator
Moderator
50 replies posted 50 sign-ins 25 solutions authored

Hi yuejin,

As I don't have a CYT2B9 chip right now, I'm testing your code on CYT2B7, where 0x14019de4  is not a valid address in workflash. So I choose another address to test, which is  0x14012de4.

There is one potential problem in your code, which is the 

numOfWordsToBeChecked = 0x1u;

You should check the whole sector instead of a word. In other word, CY_WFLASH_LG_SBM_SIZE or CY_WFLASH_SM_SBM_SIZE depending on which region you are trying to access. 

After changing this line of code to the following code, your code runs without any issues according to my test. 

numOfWordsToBeChecked = CY_WFLASH_SM_SBM_SIZE (as mentioned, the address I am using is 0x14012de4)

You can check it on your device.

Best Regards,

Finn

0 Likes
yanf
Moderator
Moderator
Moderator
50 replies posted 50 sign-ins 25 solutions authored

By the way, you don't need to change your address to 0x14012de4. Just keep using your previous address 0x14019de4.

The reason I did so is that my device is a smaller flash variant and 0x14019de4 is invalid to me.

 

BR,

Finn

0 Likes
Bill-li
Level 1
Level 1
5 sign-ins First reply posted First question asked

我估计是ECC错误导致的。这玩意儿一般处理方式就是先做Blank Check 如果Check失败就直接擦除

0 Likes
yanf
Moderator
Moderator
Moderator
50 replies posted 50 sign-ins 25 solutions authored

Hi Bill-li,

尝试读取Blank区域确实会导致ECC错误。但yuejin已经做了blankcheck显示为non-blank已写入,这种情况应该不会触发ECC错误。

Anyway,先擦除再使用Flash是一个最保险的使用方法。谢谢你的建议

Best Regards,

Finn

0 Likes