Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lukasw
Level 1
Level 1
10 sign-ins 5 sign-ins First reply posted

Hello,
we have an application using a CYT4BB µC. I'm trying to toggle an SPI driver IC with a simple 50% duty cycle signal.

I've found the following example code in AN220224:

I changed the CNT value to 36, since I'm measuring the signal on pin 12.0. Is there any configuration parameter missing?

 

 

#include "Header/cy_project.h"

#define TCPWMx_GRPx_CNTx_PWM TCPWM0_GRP0_CNT36
#define PCLK_TCPWMx_CLOCKSx_PWM PCLK_TCPWM0_CLOCKS36
#define TCPWM_PERI_CLK_DIVIDER_NO_PWM 0ul
#define TCPWMx_PWM_PRESCALAR_DIV_x CY_TCPWM_PWM_PRESCALER_DIVBY_128 // 2,000,000 / 128 = 15,625Hz
#define TCPWMx_PERIOD 0x1000ul // 15,625Hz / 4096 (0x1000) = 3.815Hz (PWM frequency)
#define TCPWMx_COMPARE0 0x800ul // 0x800 / 0x1000 = 0.5 (PWM duty)


/* Provided config struct */
cy_stc_tcpwm_pwm_config_t const MyPWM_config =
{
    .pwmMode = CY_TCPWM_PWM_MODE_PWM,
    .clockPrescaler = TCPWMx_PWM_PRESCALAR_DIV_x,
    .debug_pause = false,
    .Cc0MatchMode = CY_TCPWM_PWM_TR_CTRL2_CLEAR,
    .OverflowMode = CY_TCPWM_PWM_TR_CTRL2_SET,
    .UnderflowMode = CY_TCPWM_PWM_TR_CTRL2_NO_CHANGE,
    .Cc1MatchMode = CY_TCPWM_PWM_TR_CTRL2_NO_CHANGE,
    .deadTime = 0ul,
    .deadTimeComp = 0ul,
    .runMode = CY_TCPWM_PWM_CONTINUOUS,
    .period = TCPWMx_PERIOD - 1ul,
    .period_buff = 0ul,
    .enablePeriodSwap = false,
    .compare0 = TCPWMx_COMPARE0,
    .compare1 = 0ul,
    .enableCompare0Swap = false,
    .enableCompare1Swap = false,
    .interruptSources = 0ul,
    .invertPWMOut = 0ul,
    .invertPWMOutN = 0ul,
    .killMode = CY_TCPWM_PWM_STOP_ON_KILL,
    .switchInputMode = 3ul,
    .switchInput = 0ul,
    .reloadInputMode = 3ul,
    .reloadInput = 0ul,
    .startInputMode = 3ul,
    .startInput = 0ul,
    .kill0InputMode = 3ul,
    .kill0Input = 0ul,
    .kill1InputMode = 3ul,
    .kill1Input = 0ul,
    .countInputMode = 3ul,
    .countInput = 1ul,
};



int main(void)
{

  uint32_t sourceFreq = 80000000ul;
  uint32_t targetFreq = 2000000ul;
  uint32_t divNum = (sourceFreq / targetFreq);

  /* Assign a programmable divider for TCPWM0_GRPx_CNTx_COUNTER */
  Cy_SysClk_PeriphAssignDivider(PCLK_TCPWMx_CLOCKSx_PWM, CY_SYSCLK_DIV_16_BIT, TCPWM_PERI_CLK_DIVIDER_NO_PWM);
  /* Sets the 16-bit divider */
  Cy_SysClk_PeriphSetDivider(CY_SYSCLK_DIV_16_BIT, TCPWM_PERI_CLK_DIVIDER_NO_PWM, 0u, (divNum-1ul));
  /* Enable the divider */
  Cy_SysClk_PeriphEnableDivider(CY_SYSCLK_DIV_16_BIT, TCPWM_PERI_CLK_DIVIDER_NO_PWM, 0u);
  /* Initialize TCPWM0_GRPx_CNTx_PWM_PR as PWM Mode & Enable */
  Cy_Tcpwm_Pwm_Init(TCPWMx_GRPx_CNTx_PWM, &MyPWM_config);
  Cy_Tcpwm_Pwm_Enable(TCPWMx_GRPx_CNTx_PWM);
  Cy_Tcpwm_TriggerStart(TCPWMx_GRPx_CNTx_PWM);

  for(;;);
}

 

 

 

0 Likes
1 Solution
JJack
Level 5
Level 5
Associated Partner - Distributor Rutronik
5 questions asked 25 likes received 100 sign-ins

Hi lukasw,

yes, I agree, in CYT4BB there is only TCPWM0. Do you use the compiler from IAR and the standard driver library SDL from Infineon?

P12_0_TCPWM0_LINE36 is defined in the gpio-header file in the SDL:

JJack_0-1674577069168.png

The value is 8 and 8 selects ACT#0 from the high speed IO matrix, which is connected to PWM0_36 according to Table 13-1 in the datasheet.

Instead of P12_0_TCPWM0_LINE36 you could also use the name HSIOM_SEL_ACT_0 (which is also 8 but then the code becomes less readable.

But you have to configure the port pin, otherwise you will not have a signal output from the timer on a pin!

Regards

JJack

View solution in original post

0 Likes
6 Replies
JJack
Level 5
Level 5
Associated Partner - Distributor Rutronik
5 questions asked 25 likes received 100 sign-ins

Hi lukasw,

when you change the TCPWM counter you have to change the clock source as well:

#define PCLK_TCPWMx_CLOCKSx_PWM PCLK_TCPWM0_CLOCKS36

JJack_0-1674490207535.png

Regards

JJack

0 Likes
lukasw
Level 1
Level 1
10 sign-ins 5 sign-ins First reply posted

Hey JJack thank you I've fixed that.

However, I still don't measure an output on pin 12. My debugger shows that CNT36 is configured and enabled, and I'm idling in the for loop.

0 Likes
JJack
Level 5
Level 5
Associated Partner - Distributor Rutronik
5 questions asked 25 likes received 100 sign-ins

Hi lukasw,

you have to configure Port 12.0 so that you can measure the signal output of the PWM on Port 12.0:

/* TCPWM_LINE */
#define TCPWMx_LINEx_PORT GPIO_PRT12
#define TCPWMx_LINEx_PIN 0ul
#define TCPWMx_LINEx_MUX P12_0_TCPWM0_LINE36

cy_stc_gpio_pin_config_t pin_cfg1 =
{
.outVal = 0ul,
.driveMode = CY_GPIO_DM_STRONG_IN_OFF,
.hsiom = TCPWMx_LINEx_MUX,
.intEdge = 0ul,
.intMask = 0ul,
.vtrip = 0ul,
.slewRate = 0ul,
.driveSel = 0ul,
};

/*------------------------------*/
/* Port Configuration for TCPWM */
/*------------------------------*/
Cy_GPIO_Pin_Init(TCPWMx_LINEx_PORT, TCPWMx_LINEx_PIN, &pin_cfg1);

Regards

JJack

0 Likes
lukasw
Level 1
Level 1
10 sign-ins 5 sign-ins First reply posted

I can only find line 36 when using TCPWM1 module

P12_0_TCPWM1_LINE36  = 8,
:
P12_0_TCPWM0_LINE513 = 22,

 However, there is no TCPWM1_GRP0_CNT36 and  PCLK_TCPWM1_CLOCKS36 macro, only for TCPWM0.

0 Likes
JJack
Level 5
Level 5
Associated Partner - Distributor Rutronik
5 questions asked 25 likes received 100 sign-ins

Hi lukasw,

yes, I agree, in CYT4BB there is only TCPWM0. Do you use the compiler from IAR and the standard driver library SDL from Infineon?

P12_0_TCPWM0_LINE36 is defined in the gpio-header file in the SDL:

JJack_0-1674577069168.png

The value is 8 and 8 selects ACT#0 from the high speed IO matrix, which is connected to PWM0_36 according to Table 13-1 in the datasheet.

Instead of P12_0_TCPWM0_LINE36 you could also use the name HSIOM_SEL_ACT_0 (which is also 8 but then the code becomes less readable.

But you have to configure the port pin, otherwise you will not have a signal output from the timer on a pin!

Regards

JJack

0 Likes
lukasw
Level 1
Level 1
10 sign-ins 5 sign-ins First reply posted

Thank you very much. The problem was that the wrong GPIO file was included in the project. We are not using IAR, GHS, … rather, build using VS Code and command line.


Line number, group and count have the following relationship:

LINEx: x = (256 * GrpNum) + (CntNum)

 

 

I'm now using the following configuration and everything works.

/* PWM Mode Configuration def */
#define TCPWMx_GRPx_CNTx_PWM            TCPWM0_GRP0_CNT36
#define PCLK_TCPWMx_CLOCKSx_PWM         PCLK_TCPWM0_CLOCKS36
#define TCPWM_PERI_CLK_DIVIDER_NO_PWM   0u

#define TCPWMx_PWM_PRESCALAR_DIV_x      CY_TCPWM_PWM_PRESCALER_DIVBY_128  // 2,000,000 / 128 = 15,625Hz
#define TCPWMx_PERIOD                   0x1000    // 15,625Hz / 4096 (0x1000) = 3.815Hz (PWM frequency)
#define TCPWMx_COMPARE0                 0x800     // 0x800 / 0x1000 = 0.5 (PWM duty)   

// LINEx: x = (256 * GrpNum) + (CntNum)
/* TCPWM_LINE0 */
#define TCPWMx_LINEx_PORT                GPIO_PRT12
#define TCPWMx_LINEx_PIN                 0u
#define TCPWMx_LINEx_MUX                 P12_0_TCPWM0_LINE36

 

0 Likes