Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
GlJe_1688511
Level 4
Level 4
Distributor
100 sign-ins 10 likes given 50 questions asked

Hello.

 

I wish to know if the TRAVEO II supports the Pulse Per Second(PPS) pin of ethernet AVB.

 

Thanks and Best regards.

Glenn.

0 Likes
1 Solution
KumarAP
Moderator
Moderator
Moderator
250 sign-ins 50 solutions authored 100 replies posted

Hi Glenn,

In continuation of last reply, below are more findings : 

  • Regarding ETHx_ETH_TSU_TIMER_CMP_VAL pin:
    This signal is asserted high when the upper 70 bits of TSU timer count value are equal to programmed comparison value defined by the following MMIO registers.
    tsu_nsec_cmp[21:0]
    tsu_sec_cmp[31:0]
    tsu_msb_sec_cmp[15:0]
  • Regarding supporting the Pulse Per Second(PPS) pin :
    This IP does not support PPS only by HW, because ETHx_ETH_TSU_TIMER_CMP_VAL pin signal triggers only once.
    However, if SW change the programmed comparison value after ETHx_ETH_TSU_TIMER_CMP_VAL is asserted, ETHx_ETH_TSU_TIMER_CMP_VAL pin can be asserted every fixed period.
    If this behavior is fulfilled PPS requirement, it can be used as PPS pin.

Thank you.

Regards,

Apurva

View solution in original post

4 Replies
GlJe_1688511
Level 4
Level 4
Distributor
100 sign-ins 10 likes given 50 questions asked

Hello.

I means the AVB PPS Pulse Output pin.

It is for checking the AVB gPTP synchronization.

Thanks and Best regards.

Glenn.

0 Likes
GlJe_1688511
Level 4
Level 4
Distributor
100 sign-ins 10 likes given 50 questions asked

Hello

And, Could you explained about ETHx_ETH_TSU_TIMER_CMP_VAL pin?

Thanks and Best regards.

Glenn.

0 Likes
KumarAP
Moderator
Moderator
Moderator
250 sign-ins 50 solutions authored 100 replies posted

Hi Glenn,

In continuation of last reply, below are more findings : 

  • Regarding ETHx_ETH_TSU_TIMER_CMP_VAL pin:
    This signal is asserted high when the upper 70 bits of TSU timer count value are equal to programmed comparison value defined by the following MMIO registers.
    tsu_nsec_cmp[21:0]
    tsu_sec_cmp[31:0]
    tsu_msb_sec_cmp[15:0]
  • Regarding supporting the Pulse Per Second(PPS) pin :
    This IP does not support PPS only by HW, because ETHx_ETH_TSU_TIMER_CMP_VAL pin signal triggers only once.
    However, if SW change the programmed comparison value after ETHx_ETH_TSU_TIMER_CMP_VAL is asserted, ETHx_ETH_TSU_TIMER_CMP_VAL pin can be asserted every fixed period.
    If this behavior is fulfilled PPS requirement, it can be used as PPS pin.

Thank you.

Regards,

Apurva

KumarAP
Moderator
Moderator
Moderator
250 sign-ins 50 solutions authored 100 replies posted

Hi Glenn,

As per initial analysis, It is observed that there is no specific Pulse Per Second(PPS) output pin of ethernet AVB.
And ETHx_ETH_TSU_TIMER_CMP_VAL pin is used as "Ethernet time stamp unit timer compare indication line".

I will look more and update you accordingly.

Thank you.

Regards,
Apurva

0 Likes