Failed to load the CPU core driver Session aborte

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
dongliu
Level 2
Level 2
5 sign-ins 5 replies posted First solution authored

Hi infienon,

   I'm download active application failed .

dongliu_0-1647222161206.png

 

 

0 Likes
2 Replies
PatrickEganland
Level 1
Level 1
5 questions asked 5 sign-ins First reply posted

I had got the same problem as yours.
Have you solved this problem?
If you have solved it.
Could you tell me the method?

Best Regards,

0 Likes
KB
Moderator
Moderator
Moderator
10 solutions authored 50 sign-ins 25 replies posted

Hello Dongliu,

Before downloading please make sure :

1. If appropriate device is selected in General Options->Target->Device.

2. Appropriate Debugger Driver is selected. The CMSIS-DAP is only supported on SK boards(like CYTVII-B-E-1M-SK).

3. If you are using SK and have selected CMSIS-DAP as your debugger then change the option to CMSIS DAP->Interface->SWD

4. Check if you the traveo kit is connected to the appropriate supply voltage. (If you are using SK, then check on-board Power LED is switched ON as soon as you have connected the USB power supply).

5. If above steps do not work then close if multiple instances of IAR IDE is open(recommend to restart your system). And also try changing the option(if debugger is CMSIS DAP)  CMSIS DAP->Setup->Reset->Hardware, test if it works. 

Thank you.

Regards,
KB

0 Likes