Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

TRAVEO™ T2G Forum Discussions

Leo_Liu
Level 2
Level 2
10 replies posted 10 sign-ins 5 replies posted

Hi Sir,

目前在选择Auto MCU,参数需求具体如下,我对比了datasheet,CYT2B64BAS这个型号是否满足?或者是否有更合适的料号,请帮忙推荐下,谢谢。

PIN脚数量

80PIN

位数

32bit/16bit

Core Frequency

32MHZ

Flash

256KB

RAM

24KB

Data Flash Erase Sector Size

Prefer 256 bytes or less

Data Flash Max Erase Cycles

100 000

Data Flash

8KB

HS CAN

1ch

LIN

1ch

SPI

1ch

IIC

1ch

Analog (ADC)

10ch(精度10bit以上)

PWM

6ch

脉冲捕获

2ch

WakeUP

1ch

工作电压

5V

Deep Sleep Configurable

YES

Standby Mode&Current25℃)

≤40uA

端口带钳位二极管

YES

每个I/O端口的最大驱动电流ID

至少3路≥10mA其他≥2.5 mA

0 Likes
1 Solution
HongyanW_86
Moderator
Moderator
Moderator
100 solutions authored 100 replies posted 50 solutions authored

Hello,

根据你列出的参数,CYT2B64 除了下面几个参数需要根据客户具体要求评估,其它都满足要求的:

--Data Flash Erase Sector Size:Data (Work) Flash sector size有两种:2-KB和128-B。

--Standby Mode&Current25℃):我们的睡眠模式有deepsleep模式和Hibernate模式两种。请参考数据手册SID59A和SID62了解Spec值和相应的条件。具体模式的区别请参考Traveo II Achitecture TRM.

--每个I/O端口的最大驱动电流ID:请参考Table 26-1的IOL SPEC.对于10MA的要求,需要看客户具体什么IO应用。

CYT2B6数据手册还是PRELININARY版本,对于一些TBD或者没有的参数请联系我们销售部门,抱歉论坛里我无法提供更多信息。

Best regards,

Amy

View solution in original post

0 Likes
1 Reply
HongyanW_86
Moderator
Moderator
Moderator
100 solutions authored 100 replies posted 50 solutions authored

Hello,

根据你列出的参数,CYT2B64 除了下面几个参数需要根据客户具体要求评估,其它都满足要求的:

--Data Flash Erase Sector Size:Data (Work) Flash sector size有两种:2-KB和128-B。

--Standby Mode&Current25℃):我们的睡眠模式有deepsleep模式和Hibernate模式两种。请参考数据手册SID59A和SID62了解Spec值和相应的条件。具体模式的区别请参考Traveo II Achitecture TRM.

--每个I/O端口的最大驱动电流ID:请参考Table 26-1的IOL SPEC.对于10MA的要求,需要看客户具体什么IO应用。

CYT2B6数据手册还是PRELININARY版本,对于一些TBD或者没有的参数请联系我们销售部门,抱歉论坛里我无法提供更多信息。

Best regards,

Amy

0 Likes