Dears,
我基于CYT2B7_M4在测试TCPWM0的capture功能,例程是TVII_Sample_Driver_Library_7.2.0\tviibe1m\src\examples\tcpwm\capture,按照例程将P12.4成功修改成TC0_40_TR0复用功能,但是这个PIN也可以配置为TC0_39_TR1,尝试修改为TC0_39_TR1失败,请问该如何修改,修改了main_cm4.c如下代码:
Line28~30
/* Capture Mode Configuration def */
#define TCPWM0_GRPx_CNTx_CAPTURE TCPWM0_GRP0_CNT39//TCPWM0_GRP0_CNT0
#define PCLK_TCPWM0_CLOCKSx_CAPTURE PCLK_TCPWM0_CLOCKS39//PCLK_TCPWM0_CLOCKS0
#define TCPWM_PERI_CLK_DIVIDER_NO_CAPTURE 0u
Line33~35
#define TCPWM_TR_ONE_CNT_INx_PORT GPIO_PRT12//GPIO_PRT6
#define TCPWM_TR_ONE_CNT_INx_PIN 4ul//1u
#define TCPWM_TR_ONE_CNT_INx_MUX P12_4_TCPWM0_TR_ONE_CNT_IN118//P6_1_TCPWM0_TR_ONE_CNT_IN0
Line165~170
cy_stc_sysint_irq_t irq_cfg =
{
.sysIntsrc=tcpwm_0_interrupts_39_IRQn,//tcpwm_0_interrupts_0_IRQn,
.intIdx = CPUIntIdx3_IRQn,
.isEnabled = true,
};
已解决! 转到解答。
Hi jajic_1695691,
In SDL cpature example, you can find the TR_ONE_CNT_INx equation on the top
(TR_ONE_CNT_INx: x = (256 * GrpNum * 3) + (CntNum * 3) + TR_ONE_CNT_NR_USE)
if you would like to use "P12_4_TCPWM0_LINE_COMPL39", given GrpNum = 0 and CntNum = 39, therefore TR_ONE_CNT_NR_USE input trigger should be equal to 1.
for more information, please refer to AN220224 section 2.2.2 Table 5.
Best regards,
Hi jajic_1695691,
In SDL cpature example, you can find the TR_ONE_CNT_INx equation on the top
(TR_ONE_CNT_INx: x = (256 * GrpNum * 3) + (CntNum * 3) + TR_ONE_CNT_NR_USE)
if you would like to use "P12_4_TCPWM0_LINE_COMPL39", given GrpNum = 0 and CntNum = 39, therefore TR_ONE_CNT_NR_USE input trigger should be equal to 1.
for more information, please refer to AN220224 section 2.2.2 Table 5.
Best regards,