what is the difference between "CYTVII-B-E-176-SO" and "CYTVII-B-E-1M-176-CPU" and "CYTVII-B-E-2M-176-CPU"

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
MF
Level 1
Level 1
First reply posted First question asked Welcome!

 

what is the difference between those three boards, I Understand that all of them are socketed body evaluation board.

so 

1- Are the evaluation boards themselves compatible and the changes are related only to the chip(Microcontroller) it self which could be replaced?

2-what are the differences between the microcontrollers if any ?

3-why I can't find a link to buy the "CYTVII-B-E-2M-176-CPU"?

4-for each one of the below items does they come with their corresponding  microcontroller or it is being purchased separately?

 

MF_1-1633550520224.png

 

0 Likes
1 Solution
Apurva_S
Moderator
Moderator
Moderator
100 likes received 500 replies posted 250 solutions authored

Hi @MF 

Please see our response to your questions below - 

What is the difference between those three boards (CYTVII-B-E-176-SO, CYTVII-B-E-1M-176-CPU and  CYTVII-B-E-2M-176-CPU)

CYTVII-B-E-176-SO : It is the socketed evaluation board for TVII Body Entry family. It has a 176 pin socket that supports the TVII CYT2B7 series Flash 1M 176pin LQFP Device. This information is present in the landing page of the board.

CYTVII-B-E-1M-176-CPU : It is a non socketed evaluation board for TVII Body Entry family. It has the Traveo II CYT2B7 series Flash 1M 176pin LQFP Device soldered directly on to the PCB. Product landing page.

>> Functionally, the CYTVII-B-E-1M-176-CPU and CYTVII-B-E-176-SO boards are identical, except that the device can be easily replaced in the latter. This information is given in evaluation board user guide on page 5.

CYTVII-B-E-2M-176-CPU : This is also a non socketed evaluation board for TVII Body Entry family. It comes with a Traveo II CYT2B9 series Flash 2M 176pin LQFP Device soldered on it. Landing page.

1- Are the evaluation boards themselves compatible and the changes are related only to the chip(Microcontroller) it self which could be replaced? Functionally, the CYTVII-B-E-1M-176-CPU and CYTVII-B-E-176-SO boards are identical, except that the device can be easily replaced in the latter. This information is given in evaluation board user guide on page 5.

2-what are the differences between the microcontrollers if any ? CYTVII-B-E-1M-176-CPU and CYTVII-B-E-176-SO both have the CYT2B7 chip. CYTVII-B-E-2M-176-CPU has CYT2B9 chip. You can get the datasheet for both these devices from here. (Go to 'Products' tab)

3-why I can't find a link to buy the "CYTVII-B-E-2M-176-CPU"? Kindly contact your local sales office in this regard. You can find the details of sales offices here.

4-for each one of the below items does they come with their corresponding  microcontroller or it is being purchased separately? All boards (socketed/non socketed) come with a microcontroller already in place.

 

 

Regards.

 

View solution in original post

0 Likes
3 Replies