TRAVEO™ T2G Forum Discussions
We are looking for an MPU socket with below part number to use on a customer's prototype board.
・CYT4BFBDJS (272pin BGA)
Could you please tell me the supported socket part number of this MCU?
Thank you & Best regards,
顧客の試作基板上で使用するための、下記型番のMPUソケットを探しています。
・CYT4BFBxJSに (272pin BGA)
このMCUに対応するソケットの型番を教えて頂けますでしょうか?
よろしくお願い致します。
Show LessHello Infineon Team,
ICU Elapsed time API is not reading properly during low frequency input signal. such as (10 HZ to 130 HZ) but the tick values are providing correctly for above 130 HZ input frequency Please find the configuration details here.
MCU Configuration details: -Channel Tick Frequency - 8 MHZ of ICU Channel
Clock Reference Point Frequency - 16 MHZ
PClock frequency - 80 MHZ
Kindly let me know is there any limitations in the input signal. or should I modifications in clock configurations?
Show Less
Hello,
We would like to use the low power mode of the CYT2B73. eco We have connected an external crystal of 16MHZ, do we need to connect an external low frequency crystal to the WCO pin and then configure it through software?
After checking the DEMO file for the MUC, it doesn't have WCO connected to it, but only the ECO pin does it enable low power mode?
For SLEEP and DEEPSLEEP mode what is the difference between the two?
If you go to low power, are the clocks all off and how do you wake up the MCU?
Above.
Thank you~
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/TRAVEO-T2G/CYT2B73%E7%9A%84%E4%BD%8E%E5%8A%9F%E8%80%97%E4%B8%8E%E6%97%B6%E9%92%9F%E6%99%B6%E6%8C%AFECO-amp-WCO/td-p/738107
Show LessHi Team,
I'm currently working with the CTY4DN microcontroller.
I'm utilizing the Cy_GPIO_SetHSIOM(base, pinNum, hsiom) API, which requires passing the port number as an argument.
To obtain the port number, I'm using the Cy_GPIO_PortToAddr(uint32_t portNum)function.
However, after referring to the CTY4DN driver files, I couldn't find the expected functionality.
Could someone provide guidance on how to correctly obtain the port number?
Thank you.
Show LessHi Team,
I have a question regarding the availability of the cyhal layer for the CYT4DN microcontroller.
Can someone confirm if this microcontroller supports the cyhal layer?
If so, could you please provide the necessary cyhal layer files? Thank you.
Show Less
Hello Experts,
I was able to work with Evaluation board (TRAVEO II T2G KIT_B_E_LITE) which has MCU of CYT2BL5CAA using IAR workbench.
I used the T2G_Sample_Driver_Library_7.9.0\tviibe4m for initial configuration and i could see the LEDs are blinking.
I have a custom board which uses CYT2b95CAC chipset. I tried using the same configuration has of evaluation board(CYT2BL5CAA) and changed the only LED port pins, Flashing was successful but unfortunately no LEDs were blinking.
FYI.. I am using tviibe4m_flash_cm0plus_template from T2G_Sample_Driver_Library_7.9.0\tviibe4m\tools\iar\flash
My questions are
1. Can i use the IAR workbench template of CYT2BL5CAA to CYT2b95CAC controller( both are dual core).
2. Is there any specific configuration i need to follow for this CYT2b95CAC.
3. I am suspecting Oscillator configuration needs to be tuned as in custom board we are using 20Mhz crystal whereas in evaluation board it was 16Mhz.
Thanks
Kiran
Show LessHi All,
What will be the status of CPUSS_DP_STATUS register in Traveo II BH after executing TransitionToSecure whether the
CPUSS_DP_STATUS.SWJ_CONNECTED will be set to not active?
I am trying to reenable the DAP protection after TransitionToSecure so I am writing CPUSS_AP_CTL registers to enable the AP_CTL registers. I need to know how to confirm JTAG is enabled?
Whether the status will be reflected in CPUSS_DP_STATUS register?
Hello.
Regarding 3DL After entering deepsleep, the MCU current is around 4mA when measured separately. Both cores executed Cy_SysPm_DeepSleep to confirm that the MCU entered DeepSleep. what could the high current be related to?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/TRAVEO-T2G/3DL-deepsleep-%E7%94%B5%E6%B5%81/td-p/724510
Show Lesswhat is processor header file for cyt4bf8cds controlle.