TRAVEO™ II

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
hoop4g
TRAVEO™ II
Hello Team Infineon, I am here to ask for your recommendation onthe best  dev kit or Evaluation Board that comes with touchscreen kit orInfineon MCU t... Show More
KIM-MANSEOK
TRAVEO™ II

How can I get the code snippets, SDL, and tools used in AN228680?

Have a nice day.

 

Akhileswar_B
TRAVEO™ II
Issue :: Precision of the frequency measured is affected at higher rates of input(example: 2KHz) I am using a input tick frequency of 62500 in my ICU ... Show More
ReitA
TRAVEO™ II
Hello, I have the problem that I have to wakeup from DeepSleep Mode over Can.I'm using the CANFD0 Channel #1 with the adress of 0x40520200. The proble... Show More
WoHa_955446
TRAVEO™ II
Dears. I tried to compile my SDL1.7.1 project (CYT2B7) with MCAL1.9.0 in Greenhills but i got the following error esepcially in sram.gpj .     [el... Show More
chme_4646286
TRAVEO™ II
基于CYTVII-B-E-1M-SK验证SDL7.3 TCPWM timer功能,示例代码路径如下: T2G_Sample_Driver_Library_7.3.0\tviibe1m\src\examples\tcpwm\timer 附件是验证的cm4代码(“tviibe1m_flash_cm4_m... Show More
Venkatesh
TRAVEO™ II

Hi All,

Is there any way by which we can directly jump to M4 core by bypassing M0 core in Traveo II CYT2BL.

 

ICH
TRAVEO™ II
Hello, MCU: CYT2B7 according to the Traveo II TRM (revision H)paragraph: 31.4.1 Preconditioning - this is a safe diagnostic feature, which verify the ... Show More
rloader
TRAVEO™ II
Looking at the CYT4BB clocking diagrams, the only > 1MHz clock option for the watchdogs (WDT, MCWDT) appears to be the ECO. This is a problem for me, ... Show More
Venkatesh
TRAVEO™ II
Hi All, Is there any method using which we can run only CM4 core in Traveo II CYT2BL5Cxx board. Currently the CM0+ code is flashed using the .out file... Show More
Board Information

TRAVEO™ II

Discussion forum regarding 32-bit TRAVEO™ II Microcontroller - based on ARM® for automotive body electronics applications; cutting-edge performance, safety, and security features topics.
Top liked authors