Switches (Magnetic sensors) Forum Discussions
Dear All.
I'm using TLE4999c8 with development kit. (Eval kit vers: 2.1.1.40222).
When I flash EEPROM, no issue. When I tried to enable the 3.3V parameter, it lead to EEPROM fail (wrong values of several parameter such as Gain & Offset).
My UT is 1µs, so according user manual, 3.3V can be enable.
Attached is the dump without and with 3.3V parameter. Have you already had same issue?
Thank you for your support.
Show LessHi,
we got a problem with an PGSIS-2 Box, it has telegramm response errors.
The in the original built-in box is a version 3.3.1. But we have only a version 3.5.3 in stock
So I replaced the the old one with the 3.5.3. But it dosen´t work with our software... new error: „Get2send resault_change fromPGSISI-2 Error occurred“
My Question! Is it possible to downgrade the pgisis box from 3.5.3 to 3.3.1?
thanks for your help
Show Less
Thank you for your kind reply.
If our company pays for Hall Sensor(TLE49641KXTSA1), are you willing to obtain UL specifications for the product?
- UL Safety Specification Certification Certificate
If it is possible, please let us know what we should do.
Please Check. Thank you
Show LessDear all,
i'm using the TLE4959 with a pullup of 2,7kohm of Rload with 12V of supply voltage.
Is there a limit condition of growth of Rload for the correct operation of the transducer?
Thanks in advance
Claudio
Show LessI'm using an infineon TLE4941plusC hall effect sensor to measure speed of a rotating shaft. I was wondering if there was any information available on the recommended dimensions of the target wheel?
Show LessDear Community memebers,
TLE4999C8 requires a programming pulse (beside SICI communication) to store EEPROM content. On which pin of the IC do I need to apply the programming pulse? The datasheet and user manual does not contain this information.
Thanks in advance for the help!
Show LessHello.
I would need the evaluation board and GUI SW for the TLE4999C8. I did not found any information on it on TLE4999C's webpage...
(I already have PGSISI-2 and 3 boxes. I used it for TLE4997 and TLE4999i3 ).
Thank you.
Show LessI have no idea how to use SICI interface. I want to learn it. In my project, i will use TLE4993I3 hall sensor and i should learn how to use sensor in my circuit and how to pragramme it?
Show Less