TLE4999C8 and evaluation kit

Announcements

Measure CO2 When It Matters - Infineon’s XENSIV™ PAS CO2 now comes in SparkFun Red. Check it now!

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
JTEKTGui
Level 1
Level 1
5 replies posted 5 sign-ins First reply posted

Dear All.

 

I'm using TLE4999c8 with development kit. (Eval kit vers: 2.1.1.40222).

When I flash EEPROM, no issue. When I tried to enable the 3.3V parameter, it lead to EEPROM fail (wrong values of several parameter such as Gain & Offset).

My UT is 1µs, so according user manual, 3.3V can be enable.

Attached is the dump without and with 3.3V parameter. Have you already had same issue?

 

Thank you for your support.

0 Likes
1 Solution
Sunil_P
Moderator
Moderator
Moderator
10 likes given 25 solutions authored 10 likes received

Hi @JTEKTGui ,

As shown in the image below, for 3.3 V EN feature the SPC unit time should be greater than 1 µs (UT  1). 

Sunil_0-1679303691383.png

Also, according to the application circuit implementation, the bus line capacitor should be 2.2 nF for
UT  1us, which is not close to 0.47 nF (your implementation).
Note the pull-up resistor RP, which is typically 2.2 kΩ.

Sunil_1-1679303898722.png  

Regards,
Sunil.

View solution in original post

0 Likes
5 Replies
Sunil_P
Moderator
Moderator
Moderator
10 likes given 25 solutions authored 10 likes received

Hi @JTEKTGui ,

We are looking into your query and will get back to you soon.

Regards,
Sunil.

0 Likes
lock attach
Attachments are accessible only for community members.
JTEKTGui
Level 1
Level 1
5 replies posted 5 sign-ins First reply posted

Hello.

 

Thank you for your reply.

In fact I'm not using this board. TLE4999C8 are directly connected to the eval board. I have a PCBA with TLE4999C8 and CL capacitor between pin 4 & 3 of TLE. The capacitor value is 470pF (so less than what is required for 1µs UT).

I only have issue for EEPROM programing when 3.3VEN parameter is enable.

 

Thank you.

0 Likes
Sunil_P
Moderator
Moderator
Moderator
10 likes given 25 solutions authored 10 likes received

Hi @JTEKTGui,

Can you please attach the image of your setup/ application circuit once, it will be helpful.
And you are programing EEPROM through GUI, right? 

Regards,
Sunil.

0 Likes

Here is picture of the setup. (I'm programing EEPROM with the GUI).

For the application circuit, it is the same as in datasheet of IC. and Capacitor value on the bus line is about 470pF.

When I enable 3.3V function  and try to burn EEPROM, it failed.

IMG_20230320_070007.jpg

0 Likes
Sunil_P
Moderator
Moderator
Moderator
10 likes given 25 solutions authored 10 likes received

Hi @JTEKTGui ,

As shown in the image below, for 3.3 V EN feature the SPC unit time should be greater than 1 µs (UT  1). 

Sunil_0-1679303691383.png

Also, according to the application circuit implementation, the bus line capacitor should be 2.2 nF for
UT  1us, which is not close to 0.47 nF (your implementation).
Note the pull-up resistor RP, which is typically 2.2 kΩ.

Sunil_1-1679303898722.png  

Regards,
Sunil.

0 Likes